Sorlox: Measuring Fusion Reactions in Real Time Sorlox: Measuring Fusion Reactions in Real Time | HBM

Measuring Fusion Reactions in Real Time Helps in Design of Unique Spiral Shaped Accelerator

To produce the same kind of clean energy that powers the sun and the stars, scientists and researchers have long tried to build nuclear fusion devices that would work here on Earth.

A recent design from research and development firm Sorlox, Inc. uses a unique spiral shaped chamber to compress fuel into a plasma state, which then ignites and generates huge pulses of energy.

To build an optimal device, the company needed to measure — in real time — data such as the currents and voltages of the electromagnetic “cage” used to control the plasma as it floats past the accelerator walls.

This posed a design problem because the extremely hot and highly electrically charged plasma reacts so quickly it could potentially be difficult to measure. In developing its device, the firm used a Genesis high-speed data acquisition system (DAQ) from HBM.

As a review, recall that nuclear fusion is a process that differs from fission, the type of atomic reactions harnessed by existing nuclear power plants.  Basically, fission produces energy by fracturing atoms, while fusion produces energy through miniscule acts of atomic coupling.  In the sun’s core, thermonuclear temperatures reach fifteen million degrees C, high enough to cause protons to slam together and unite. Each time this happens, a tiny amount of mass is lost.

As Einstein’s famous equation E=MC2 states, the mass is released in the form of energy. The released energy is explosive and totals huge amounts — thousands of times the amount it took to bind the atoms together in the first place. 

The Basic Physics

Engineers, scientists and physicists have long attempted to develop a fusion device or accelerator that would work here on Earth. Many think that the devices could help end the environmental destruction being caused by harmful byproducts from traditional energy sources.  The fear is backed up by recent statistics that claim by mid-century, the atmosphere will likely contain 500 parts per million of CO2, while towards the end of this century, the effects of this will cause major ecological harm. Renewable sources like solar and wind won’t play a significant part in solving the problem, because they fluctuate too much and are difficult to store. The hope is to harness the immense energy produced by fusion reactions.

Researchers have already built lab devices that cause fusion reactions by compressing a fuel pellet that contains deuterium (D), an isotope of hydrogen easily extracted from seawater, and tritium (T), made from lithium, also available from sea water.

Similar to what happens in the sun or a star, when deuterium and tritium nuclei are fused at high temperatures and pressures, they form a helium nucleus, a neutron – and huge amounts of energy. 

At such high temperatures, matter exists in a plasma state where electrically neutral atoms or molecules have been converted to electrically charged atoms or molecules (ions).  The hot plasma must be confined for a sufficiently long period so that it does not cool down and for fusion to occur and produce energy. 

Because the plasma is electrically charged and extremely hot, it has been found that the optimal mechanism to “cage” it is a strong magnetic field in the shape of a torus

Scientists have built devices that produce temperatures more than ten times higher than in the sun and cause fusion reactions which produce megawatts of power for a few seconds.

One project trains lasers on a tiny fuel pellet of the hydrogen isotopes deuterium and tritium. The pressure from the lasers compresses the fuel pellet which is inside of a cylinder until the deuterium and tritium fuse together, releasing a huge burst of energy.

The ongoing challenge has been to create a device where the amount of energy released by the fusion reaction is greater than the amount of energy that went into creating the fuel pellet. The next step is creating a fusion reaction that – like the reactions in the sun or stars – is self-sustaining, a point called “ignition.” In other words, the challenge is to create a self-sustaining, synthetic star.

In developing its accelerator, Sorlox attacked the problem from another direction. The first innovation was developing a spiral shaped compressor made from cast metal, which the company dubbed the Nautilus, for a more compact device about the size of a refrigerator.

Sorlox makes a plasma by taking deuterium gas and ionizing it using a high-strength magnetic field. The plasma is in the form of a current ring called a compact toroid. The magnetized plasma is launched into the Nautilus compressor and squished down from 1015 ions/cubic centimeter to 1018 ions/cubic centimeter. This is hot and dense enough to facilitate ignition. 

Measuring the Process

In running the math needed to develop the device, the scientists realized they needed a DAQ that could measure about 100 million samples per second. The Genesis DAQ employs a fast card that could handle those rates.  The first iteration of the nuclear accelerator required the use of a four channel DAQ, and the next-generation machine needed a 12 channel system.  

According to project lead Brent Freeze, Sorlox used the DAQ to measure the electromagnetic fields that control the plasma.  A special magnetic sensor in the unit read currents over a distance – important because of the pressures and temperatures involved. 

The sensor is an inductive device wrapped around an electrical conductor. Its output is a small voltage that represents the current induced as the plasma passes by.  The scientists also used the DAQ to measure the density of the plasma and its speed while it is being ejected into this compressor.  A separate high-speed camera system allowed viewing the propagation of plasma – how it forms and is compressed.

Application Implications

The DAQ took data continuously. This was important, because when each pulse is run, it must be controlled, which requires a feedback mechanism. With all the measurement data available, it was possible to determine the excitation and the responses from the different sensors to correlate all the data together.

“Everything was being recorded by the DAQ,” says Freeze. “Not only was the unit taking the data from the sensors, it was also digitally duplicating what's coming in on the cameras into linked files. The DAQ is actually doing double duty here. It’s both taking the data while we're running and also backing up all of the imaging data on a hard drive. The DAQ let us explore what happens when you take a plasma up to these extreme temperatures and magnetic fields."

According to Sorlox, the biggest application for its latest generation fusion accelerator is potentially electric power generation. Based on the annual fuel costs for a 1 GW coal-fired power plant, estimates say that a 90% fuel-cost saving is feasible using the new technology. 

Also, the technology is environmentally friendly because it emits no greenhouse gases.  Other newer models of the pulsed plasma device work in applications including medical isotope and Helium-3 production.

The DAQ continues to be useful to Sorlox in developing next-generation machines by helping engineers get better models of fusion reactions and how they work.