Electric Power Testing - From Component to Vehicle Energy Management

HBM provides the entire measurement chain for electrical power testing - from electrical machine testing to high voltage and complex inverter control testing in the automotive, ground vehicle, and aerospace industry as well as the manufacturing, production, and energy industries.

Our solution covers sensors, hardware, and software for testing electrical inverters and electrical machines. Mechanical signals (e.g. torque) and electrical signals (current and voltage) are acquired simultaneously, helping you to better understand the electric drive and its losses within minutes. This is important for the optimization of the drive as well as the increase in efficiency.


Electrical Machine & Powertrain Testing

Testing electrical machines and electrical power trains is a key task in developing the electric future of industry and transportation. ​
For a substantial increase in efficiency of next-generation machines, drives, cars and larger vehicles, it is essential that every machine and every drive are precisely tested and improved, wherever possible. And that these tests do not only cover static tests but also allow the understanding of the dynamic behaviour of machines and drives.

Electric System and Inverter System Testing

Creating a system out of components sounds easy but testing this is a real challenge. And it becomes more difficult as advanced concepts like high phase counts, multi motor drive trains or hybrid vehicles are coming into the picture. Or if the system just gets so large that investigating on component level only does not help. Be it an all-wheel electric car, a locomotive from pantograph to traction motor, or the electric installation on board a ship or a plane, testing needs to be able to adapt to these complex multi-dimensional tasks.

High Voltage and Switchgear Testing

Higher power electrical machines are operated at higher voltages and huge currents – several kV and kA. Or – like in aerospace -  voltages are brought up to bring currents down to save copper-based weight. Safely and accurately testing such machines and installations operating above the 1 kV border of “low voltages” is quite challenging. ​
And when it comes to the subsystems an AC or the new DC grids are built up from – inverters, transformers, switchgears – the demand on high voltage test capabilities up to several 100 kV as well as equipment and user protection becomes mission critical.

Grid Testing

While power is generated and distributed there is a continuous challenge to test the quality of the generation, ​
the effects from the consumers back into the grid, and the stability and quality of the grid itself. Modern grids are highly managed intelligent energy distribution systems, and advanced test methods are needed to understand the grid behavior better beyond the typical RMS and power values.

The World of Electric Power at a Glance

Please click on the green dots to learn more

Click Here For Your eDrive Brochure

What Our Customers Say About Us

This client from a large automotive OEM has procured Genesis HighSpeed DAQs directly from HBM and has specified in their key requirement document for test rigs that HBM products must be integrated by the system integrator.

“HBM is currently the best in the market … they also have good visibility of how technology is changing and are proactive in guiding us on where we need to be …”

Advanced Analysis with HBM's Electric Power Testing Solutions

HBM does not only offer best-in-class hardware for power measurements, but also provides advanced analysis tools with the leading Perception software:

  • Vibration Measurements in Electric Machines
  • Synchronized CAN bus measurements
  • dq0 transformation
  • Drive Cycle Power Measurements
  • Dynamic Power Measurements
  • Dynamic Torque Measurement
  • Torque Ripple
  • In Vehicle Electric Power Measurement
  • Space vectors

Download the PowerPoint:

Click here to receive in-depth information in a convenient PowerPoint format to share with your team or colleagues.

Become Part of the e-Power Community and Receive Tips and Tricks On How to Optimize Your Test Setup