A Simple Solution for Fast & Safe Force Measurement Tasks A Simple Solution for Fast & Safe Force Measurement Tasks | HBM

HBK Introduces the Configurable Piezoelectric Force Measurement Chain CMC

HBK has created new CMC piezoelectric force measurement chains which can be freely configured in more than 200 combinations, making them ideal for a range of industrial measuring tasks, including joining, forming or assembly processes.

Users can select a sensor that matches their required measuring force, potential initial load, and desired overload range. The selection of the amplifier depends exclusively on the force to be measured, which enables a high output signal and good resolution.

Each measurement chain comprises a sensor, a charge cable, a charge amplifier and the associated test protocol that documents the relationship between the force in Newtons and the output signal in volts. To improve user accuracy, HBK also specifies the calibration results for multiple force ranges.

Charge cables in different lengths are available to allow for easy integration. CMC force measurement chains are suitable for rapid measurements and force-displacement monitoring, as the sensor's deflection does not affect the displacement measurement. Plus, all HBK’s measurement chains meet the required IP65 degree of protection.

A switching input allows for zero-balancing of the charge amplifiers and a magnifying function can be activated to ramp up the amplifier’s sensitivity.

Sensors with nominal forces ranging from 5 kN to 120 kN are available. The charge amplifiers have input ranges between 1000 pC and 482,000 pC, with the resulting nominal measurement ranges varying from 125 N to 120 kN.
 

Marketing Coordinator

Heather Wilkins
Telephone: +44 (0) 1223 389 800
Email: [email protected]

About HBK – Hottinger, Brüel & Kjær

For many decades, HBM and Brüel & Kjær have been trusted across multiple industries to deliver highly accurate technologies and expertise in test and measurement and sound and vibration. HBM as the market leader in testing, measuring and analysis and Brüel & Kjær as the world’s leading solution provider for measuring and managing sound and vibration.

The two companies have now joined forces as HBK - Hottinger, Brüel & Kjaer to form the world’s foremost provider of integrated test, measurement, control, and simulation solutions.

For more information, please visit www.hbkworld.com