Reference temperature

In the noIn the operating temperature range the force transducer enables measurements to be taken, however, the measurement accuracy is limited.minal (rated) temperature range the force transducer meets the values given in the specifications.

Force Measurement Glossary: Characteristics of Force Transducers

Benefit from our practical on-line glossary to look up the most important technical terms in the field of force measurement:

HBMへのお問合せ HBMやHBMの製品について「もっと詳しく知りたい」、「わからないことがある」、「こんな製品を探している」などございましたら、お気軽に下記お問合せフォームでご連絡ください。