CAN Based Temperature Data Acquisition with the HBM SoMat CAN Based Temperature Data Acquisition with the HBM SoMat | HBM

Webinar: CAN Based Temperature Data Acquisition with the HBM SomatCR

 

Do you want high precision temperature data in extreme temperatures and severe conditions?  The ruggedized SomatCR can provide this  by simply connecting it through a CAN compatible network.  This webinar will discuss how to create and load a setup file for the module as well as show you how to use multiple SomatCR units within a distributed CAN network.  Using the SomatCR Assistant software, the module will be configured for use with various data acquisition systems that have CAN capability including the Somat eDAQ and the HBM QuantumX.