HBM提供のトルクセンサT22を使用して取得したデータは、InVentusが2位を獲得した際の重要な成功要因でした。センサは、ロータの動力および挙動に関するデータを直接取り出すことができるように、車両のロータの下流に直接設置しました。このデータにより、最適なブレードピッチの設定やドライバーの訓練などをはじめ、様々な改良を行うことができました。
風速の80%で2位
5ヶ国から車両9台が参加した、このレースは、向かい風を唯一のエネルギー源として、向かい風に向かって最速で走れる車両が勝者となります。シュトゥットガルト大学のチームInVentusは、風速の約80%を達成し、再び2位を獲得しました。これは、前年に比べ約25%の性能向上でしたが、カナダのチームChinookがより優れた性能で優勝しました。
トルクセンサT22で、ロータデータを収集