The correct use of accelerometers requires consideration of several factors to ensure good measurements. Factors to consider are:
- Expected vibration level
- Expected frequency range and required frequency range
- Dynamic range
- Noise floor
- Temperature
- Is the measurement location constant temperature? Rising or falling?
- What mounting method can be used?
Once the measurement is complete how should the accelerometer be removed? In this webinar, we will provide answers to these questions.