Insulation resistance

The resistance between any connecting cable and the spring element is called 'insulation resistance'. It is essential that the insulation resistance corresponds to the value at ambient temperature specified in the data sheet; otherwise the transducer needs to be replaced, since the characteristics no longer are correct.

Force Measurement Glossary: Characteristics of Force Transducers

Benefit from our practical on-line glossary to look up the most important technical terms in the field of force measurement:

1:1 문의 이곳을 클릭하셔서 요청사항을 작성해 주세요