arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management
null

Swedish Measuring Wheels – Making Trains Safer All Over the World

Interfleet uses HBM data acquisition systems to carry out rail measurements in a scalable and flexible way

Interfleet Technology, an international consultancy with a test center in Stockholm, are experts in the testing of railway vehicles – including statutory safety testing at the time of commissioning as well as troubleshooting running vehicles. Their task is to verify the running behavior – measuring all the parameters influencing the safety, the operation and, ultimately, the economics of these multi-million dollar vehicles. They have the challenge of acquiring and analyzing large volumes of measured data as efficiently and as correctly as possible, resulting in a thorough analysis of all the mechanical quantities affecting the train.

This means that data acquisition is critical for Interfleet's traveling team of experts. If you have just spent three weeks testing the railways of Sweden, India or China, the last thing you want is to return to the field because something has been missed – for example how the train behaves on a particular gradient in a curve at a particular speed under certain weather conditions on a Siberian mountain. Interfleet produce their own measuring wheel with sensors, but they also rely on HBM data acquisition systems and software, which can handle large volumes of data and allow configurations to be changed quickly and easily in the field.

Pioneers in Measuring Wheels

In the 1950s, Interfleet was part of the engineering division of SJ (Swedish State Railways), and even back then it was already a pioneer in measuring technology in the railways. The Swedish test team were the first in the world to use a measuring wheel (IWT) for rail vehicles, and they have built upon this to become world leaders today.

Next-generation measuring wheels are now in use, able to handle frequencies of up to 3 kHz (IWT4). The measuring wheels are fitted with sensors based on the very latest technology – testing factors like speed and acceleration, power, displacement and strain, parameters such as track force and stability, or wear issues like strain in the bogie frame, grooves in the track or flexural stresses in the axles. Measuring wheels for the global market are manufactured in the Interfleet lab in Solna, near Stockholm.

null
null
null

Up to 170 Measuring Points

Survey assignments are commissioned by vehicle manufacturers and owners including Siemens, Alstom, Bombardier, LKAB, Vale and Indian Railways, and Interfleet's engineers respond to them with a global solution covering the entire measuring chain. Data acquisition equipment is installed on the train along with the custom-built measuring wheels.

The data acquisition system is the QuantumX or MGCplus from HBM, with acquisition nodes in each car. The system supports on-board data monitoring and classification in real time. A large-scale survey assignment can involve as many as 160-170 measuring points, with sensors distributed around the vehicle and several pairs of measuring wheels in the trainset. They communicate with the system via optical fiber, which is laid through the cars. In large assignments, the measuring equipment may occupy several pallets, whereas it can all fit in one case in a small assignment.

Full-scale type approval can be completed in two to three weeks of traveling around the rail network. "In order to obtain all the data combinations we need for a thorough analysis, several gigabytes of data are collected every day," explains Jan Wännman, surveying expert at Interfleet in Sweden.

"By classifying the data as soon as we collect it, we can be certain that we're getting everything we need. We work on the train, in constant touch with the driver, asking for different speeds or to increase or reduce the load, making sure we cover all the necessary conditions. When we finish, we then take the data from binary files in the HBM data acquisition program catman and analyze it using the advanced mathematical program Matlab on the basis of predefined criteria – this operation can take up to a week."

null
null
null

Confidence in the System

Following the weeks spent on the rails, the Interfleet team prepares all survey assignments back in the Solna test center. Setting up a new survey assignment takes careful planning.

"When we're out in the field there are so many parameters that can go wrong or that we can't control. This could be the wind and the weather, leaves on the track, or some other problem during the short window we have to complete the survey. We have more than enough uncertainty to cope with. That's why we really need to be confident that that data acquisition system will work – and the QuantumX and MGCplus from HBM have shown that they are reliable. They also make it easy to change the survey configuration if necessary by switching channels on and off, without the need to reprogram the entire setup. This scalability and flexibility is invaluable out in the field," says Jan Wännman.
 

Related Products

No more result to load