arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Measuring temperatures at high speed: QuantumX amplifier records motor temperature at Toyota Motorsport test bench

toyota motorsport gmbh, germany

Introduction

Running at 200 mph and faster, with swift acceleration and sharp braking, long-distance auto races like France’s 24 Hours in Le Mans are endurance tests for engines. Temperature distribution plays a central role in optimizing engine performance.Toyota Motorsport GmbH, a leading automotive testing and development company that specializes in high technology, optimizes engines and boosts efficiency with its new test bench, featuring HBM’s QuantumX measurement amplifiers and  QuantumX measurement data acquisition system.

chevron_left
chevron_right

Simulating temperature distribution in the combustion engine with a new test bench

Headquartered in Cologne, Germany, Toyota Motorsport helped develop and test engines, chassis and other parts of racing cars for the Panasonic Toyota Racing Formula One team. After Toyota left the race scene in 2009, the company became a test and development center, specializing in high-technology. In 2012, it returned to international motor sports, entering a hybrid vehicle in the FIA World Endurance Championship, including the 24 Hours of Le Mans. 

Toyota Motorsport has numerous testing methods—including a wind tunnel—for different parts of vehicles. It uses the tests not just for internal development projects but also offers them to other providers in motor sports and the automotive sector. To further expand its range of offerings to outside organizations, the company decided in 2013 to set up a new combustion engine test bench for multi-point temperature measurements

This will allow us to simulate temperature distribution in the engine. With that data, engineers will then be able to optimize the cooling circuit, for example, and boost the overall efficiency of the engine, explained Bruno Kanzenbach, Senior Engineer at Toyota Motorsport. We have a lot of know-how in test benches, but for measurement technology, we prefer to rely on the expertise of specialized providers.

Rapidly and accurately measuring a high number of channels

Kanzenbach works in the chassis department and calibration laboratory, but he was given the responsibility of choosing the measurement technology because of his broad experience in metrology. He started by defining the requirements, which included the capability to provide data from at least 100 measuring points, synchronously and in real time, directly to the test bench. The measurement technology also needed to represent even the slightest temperature variationsv precisely.

"We had narrowed down our selection process to four measuring amplifier systems. Then the HBM QuantumX amplifier won us over in the practical test, especially with its extremely low measurement uncertainty," said Kanzenbach.

HBM delivered eight modules type HBM MX1609 (16-channel thermocouple measurement amplifier type K) for Toyota Motorsport. With its modularly distributable system concept, the QuantumX amplifier flexibly adapts to the number of measuring points and supports all commonly used transducer technologies. Its high measurement accuracy makes it possible to connect the thermocouple plugs directly to the device.

"There is a risk with cable clamps that the measurement will be distorted by the heat emitted from the engine into the room. That problem disappears with this connector solution," explained Kanzenbach. "This also saves us a lot of time during setup. An engine test bench is a complex structure because, in principle, it simulates a complete vehicle including the electronics, cooling circuit and exhaust. So it's quite practical if the more than 100 measuring points can be connected to the measuring amplifier simply by connector, as with the QuantumX amplifier. Then there's no need for additional cabling, which can be very extensive." Connectors also make it easy to convert the system quickly for tests on different engines.

 

Calculating temperature distribution at different loading levels with real time data

HBM technology is especially user-friendly in practical applications: Before starting up, the thermocouples are conveniently calibrated by the LabVIEW* software via an the QuantumX system's open interface. After, the thermo-transducers are distributed over the motor block, cylinder head and exhaust system and then applied at different depths of the material. The test bench runs through several operating points during the test to simulate different types of loading encountered while driving. The QuantumX amplifier records the temperatures and forwards the information to the test bench system via scalable outputs in real time.

QuantumX temperature measurement with LabVIEWTM

"Our system is integrated into the test stand measuring system through the HBM QuatumX CANbus Gateway. We have instant access to all temperature data and are able to work with the data," explains Kanzenbach. 300 temperature values per second can be recorded and transferred for each channel at a bandwidth of up to 15 Hz with 24-bit resolution, immune from interference. The thermal calibration of the measuring chain based on only two measurement points allows for a further significant improvement in measurement accuracy. This ensures that even very small dynamic temperature changes will be recorded.

Then the data is combined on the test bench with other engine values such as speed and torque. For very high speeds up to 30,000 rpm, an inertia-optimized torque measurement system is used. The results make it possible to calculate temperature distribution in the engine at different engine loading levels. "With this high-precision measurement of temperatures, engineers can then improve engine efficiency still further," concludes Kanzenbach.

* LabVIEW is a registered trademark of National Instruments Corporation.

 

 

Toyota Motorsport GmbH, a leading automotive testing and development company that specializes in high technology, optimizes engines and boosts efficiency with its new test bench, featuring HBM’s QuantumX measurement amplifiers and QuantumX measurement data acquisition system.

"We had narrowed down our selection process to four measuring amplifier systems. Then QuantumX from HBM won us over in the practical test, especially with its extremely low measurement uncertainty."Bruno Kanzenbach, Senior Engineer at Toyota Motorsport GmbH (TMG)  Learn more about Toyota Motorsport GmbH (TMG)