Precision couplings for HBM torque transducers

Couplings for torque transducers are a key accessory. A torque flange is a precision transducer that enables very small uncertainties of measurement to be attained. However, certain requirements need to be met to achieve this. One of the most important is to minimize the parasitic loads affecting the transducer which, among other things, result from alignment errors in the drive train.

Offset compensation is the main task of offset couplings

Besides precise torque transfer, the main task of a coupling consists of offset compensation. In nearly all practical applications, these offsets occur between the driving and the driven side. They result from dimensional tolerances in the components used as well as from external influences such as temperature that prevent complete elimination of the offsets.

  • Axial offset
  • Radial offset
  • Angular offset

Our video provides an example of how to use a double coupling and of how it works in the context of a torque transducer.

Our recommended suppliers

Online configuration tool for mayr precision couplings

The online configuration tool for mayr precision couplings for HBM torque transducers allows you to conveniently choose the configuration that matches your requirements and order the product in original manufacturer quality.

mayr Online Configuration Tool

Related products

TB2
Torque reference transducer which was developed as a reference and transfer transducer for use in on-site calibration.
Contacteer Gelieve contact op te nemen met HBM als u wilt ontdekken wat HBM voor u kan betekenen.
Mayr Torque Couplings

Find the right coupling for your HBM torque transducer at mayr.com