Numerical and Experimental Study of a Sailing Yacht Assisted by the Use of Strain Gauges

This study has been carried out within a framework of research activities regarding the innovative design and manufacturing of a small sailing yacht (called LED - Linen Epoxy Dinghy). These activities have been performed at the Dipartimento di Ingegneria Chimica, Gestionale, Informatica e Meccanica of the University of Palermo, in cooperation with the Facoltà di Ingegneria e Architettura of the University of Enna Kore. The purpose was to evaluate the strain field of a 15' SKIFF type sailing yacht by using strain gauges, and compare the experimental evaluation with the prediction of a Finite Element Method (FEM) model.

Due to the application of the load system, FEM results obtained from preliminary numerical simulations identified the most critical deformed areas, located in the hull (fig.1), and in transversal and longitudinal internal stiffeners (fig.2). The hull material is in particular a sandwich structure composed by Flax Reinforced Plastic skin laminates and by agglomerated cork as core. Strain components were measured on the internal skin of the hull, by means of four three-grid rosettes HBM type RY81-6/350, and a thermal compensator rosette. The sites of maximum normal strains on the transversal and longitudinal stiffeners of the yacht (made of marine plywood), were also considered, by installing four single-grid HBM strain gauges, type LY11-6/350 and a thermal compensator strain gauge.

Each single grid in all installations was wired up by using a four wires scheme, and protected with polyurethane paint from HBM type PU140 and a silicone sealing layer from HBM type SG250 (fig.3 and 4).

A load configuration was reproduced in the lab, simulating a loading scenario acting on the boat during typical sailing conditions (fig.5).

The measurement of strain gauge signals was carried out using Wheatstone bridges. The acquired signals, sampled over a time window sufficient to achieve a stabilized behavior, were then processed to obtain the complete strain state and to compare it with equivalent numerical FEM results.

The matching of experimental and numerical results was very satisfactory, allowing to conclude that the FEM model is reliable. Moreover, the confidence gained about the reliability of the measured data, has opened the way for an experimental campaign of on-site measurements, during real sailing conditions. This procedure will require the connection of a strain gauge controller with a transponder and a GPS system.

The customer

University of Palermo

The researchers:

  • Prof. Antonio Mancuso
  • Prof. Giuseppe Pitarresi
  • Mr. Giovan Battista Trinca

University of Enna Kore

The researchers:

  • Prof. Davide Tumino

Related Products

RY Strain Gauge Rosettes with 3 Measuring Grids
These strain gauge rosettes are an appropriate choice for analyzing the biaxial stress state with unknown principal strain directions.
LY Linear Strain Gauges with 1 Measuring Grid
Linear strain gauges with 1 measurement grid is the first choice for strain measurements in only one direction.
SG250 Silicon Rubber Covering Material for Sensors | Tube
SG250 covering material is a transparent silicone rubber that is applied from the tube. It cures in contact with air at room temperature.
Contacteer Gelieve contact op te nemen met HBM als u wilt ontdekken wat HBM voor u kan betekenen.