How to get the most out of your optical interrogator

 

In real optical sensing networks, losses can change over time and affect sensors differently, jeopardizing measurements.

Even if the optical interrogator has a high dynamic range, if you are not able of taking full advantage of it, you are throwing away your investment.

In this webinar, the innovative Smart Peak Detection (SPD) method that allows the accurate and stable detection of all the sensors in large/complex optical networks is explained. You also have the chance to witness a live demo of its performance in different situations, with real data being acquired using one of HBM FiberSensing's stand-alone interrogators.

After this webinar we are confident you will be willing to perform all your measurements using Smart Peak Detection.

 

This webinar was originally held on July 8, 2015.

Presenter

Filipe Magalhães

  • New Product Launch Manager
  • HBM FiberSensing
Contacteer Gelieve contact op te nemen met HBM als u wilt ontdekken wat HBM voor u kan betekenen.