arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Testing Electric Motors Under Load at "Van Bodegraven Elektromotoren"

Van Bodegraven Elektromotoren, Netherlands

Introduction

Van Bodegraven, Dutch supplier of electric motors, was able to use existing torque sensors and DAQ systems for designing a complete new test stand.

chevron_left
chevron_right

HBK Measuring Equipment Makes an "ECG" for Every Electric Motor

"Van Bodegraven Elektromotoren" in Dordrecht (the Netherlands) specializes in working with electric motors. The company supplies and installs new motors of various brands and has a workshop for carrying out repairs and overhauls. The test facility for electric motors at Van Bodegraven Elektromotoren has been using measuring equipment from HBK since 2016 to determine parameters including torque, rpm, voltage, and temperature.

“This enables us to make a sort of "ECG" for each motor,” states the manager, Richard Renee.

Van Bodegraven Elektromotoren, based in Dordrecht, is an established supplier of electric motors in the Netherlands, dealing in both new and refurbished motors. Around sixty percent of the company’s turnover comes from the maritime sector, and forty percent from the industrial sector. The motors are used for applications such as ship propulsion, as well as for driving pumps, fans, cranes, winches, anchor winches, and conveyor belts. This usually involves critical business applications, where a high level of reliability is required.

Van Bodegraven is an independent brand and supplies motors from manufacturers including ABB, Cantoni and Siemens. The company also has its own label Dormot, which comes from China. Chinese motors are somewhat more favorably priced and are mainly used for less critical applications. The make and type of motors that Van Bodegraven recommends to its clients depends largely on the application, of course.

Overhauling vs replacing electric motors

According to Richard Renee, Van Bodegraven concentrates mainly on the replacement market.

“Large new build projects have become fairly rare in recent years unfortunately, and overhauls have also become a less frequent option. We have an extensive workshop where we repair, overhaul and modify motors, which makes up some 25 percent of our turnover. Overhauling an electric motor is no longer economically feasible in many cases. Motors rated up to about 45 kW have become much cheaper in recent years, so buying a new one is generally cheaper. Overhauls are only an option in the case of special motors that are no longer available or have a long lead-time. These include multi-speed motors, DC motors, or motors with special dimensions.”

“When we replace a motor, we do it on a one-for-one basis,” Renee continues “which means that a motor for a particular application is replaced by another. Supplying motors that exactly match the requirements for the specific application is crucial in the replacement market. They have to be delivered and installed quickly, for example, aboard ships that are loading and unloading their cargo in the Port of Rotterdam for the day. This means that we have to have the most common types of motors in stock, which cover hundreds of different brands. We also supply shafts and other components. We install motors on the clients’ premises and are increasingly employed to perform maintenance as well. Most of our mechanics are very enthusiastic about their profession, and know exactly how a motor is running when they feel it and hear it. We can also see that condition monitoring and predictive maintenance are becoming more and more important. We can read a motor’s status and performance remotely and wirelessly, which enables us to plan its maintenance. In the future, we will also be able to use measured data and our knowledge to predict when a problem can occur.”

null
null
null

Test stand

Testing motors has grown in importance as a work process at Van Bodegraven. According to Renee,

“Many clients want to know in advance whether a motor meets the requirements in practice. This involves not just its performance, but also its energy efficiency, for example. We therefore brought a new, and one-hundred-percent vibration-free, test stand into use a year ago, whereby motors are tested under load in a vertical or horizontal position.”

Van Bodegraven uses torque sensors and measuring equipment from HBK in the test stand. Renee states,

“We looked closely at equipment from a number of suppliers and finally chose HBK. What is interesting is that we already bought an HBK T10F torque meter in 2004 and are still using it. It is rated at 5000 Nm. We have also bought a PMX measurement amplifier. This combination enables us to make simultaneous measurements of torque, rpm and temperature, as well as all electrical parameters such as voltage, current and power consumption. The measured data are read into the PMX modules in the analog form and are displayed on a screen using HBK’s catman Easy software, which makes the information easy for the client to understand as well. We provide them with a precise test report containing all the relevant graphs. In the new test rig, we also wanted to provide reliable measurements in the low torque range, and therefore purchased a new torque meter: the T40B with a nominal capacity of 500 Nm and with speed control. In addition to torque and speed, the meter also provides temperature, voltage and current readings and is also able to calculate energy consumption. The PMX data-acquisition and measurement system, together with the catman software from HBK, was the possible solution for our test setup. The modular nature of the measurement system, comprising of various measuring amplifier cards, renders the measurement and synchronization of all signals in the system a possibility.”

The measured values are read and digitized in the PMX measurement system. The system is then connected to a computer pre-installed with the catman software. The measured data is displayed real-time in chart forms, and visualized on the screen of the measuring chamber. This provides easily-comprehensible information for the customer, who may be observing the information over the operator’s shoulder. Besides displaying the information, the catman software also stores the measured values, allowing Van Bodegraven to calculate and assess the efficiency of the drive based on the asset data. The same data is utilized by the software to analyze trends, thereby providing the customer a comprehensive test report balence with all the relevant data.

Distinguishing capacity

Van Bodegraven’s test stand is also used a great deal by ABB, among others. ABB is a major supplier to Shell, which in turn has very demanding requirements for motors. The controllers for its motors use only Shell software; so, testing the combination of the controller and software is extremely important for motors destined for Shell plants. ABB test engineers run not only performance tests at Van Bodegraven, but also simulations and locked rotor tests. Heat run tests and endurance tests at full power can also be carried out. These tests are intended to show that the drivetrain (the motor plus the frequency controller) meets the client requirements.

Van Bodegraven has invested a great deal in this test stand. Heavy motors being tested at 100 percent load can cause severe vibration; therefore, a soil survey has been carried out to devising a way of coping with this. The result is that 12 piles have been driven as deep as 12 meters into the ground under the floor of the test stand to absorb the vibrations. This floor is not connected to the hall floor; so, the vibrations are not transmitted to the rest of the building.

In addition, Van Bodegraven can generate its own power of up to 600 kW on site (and even more with a number of adjustments), so that only losses from the mains are taken during tests.  An additional test engineer, trained by HBK to work with the software and the test equipment, has been recruited for performing the tests. HBK also takes care of the annual calibration of the torque sensors and the PMX-system. The new test stand sets Van Bodegraven apart from its competitors in the region, all of whom lack a similar capacity for testing electric motors under load. The test stand is not yet in full-time use; so, Van Bodegraven will be happy to make it available to other suppliers.

About Van Bodegraven Elektromotoren

A true family business. From the first generation to the current fourth, we believe that stagnation is decline. Energy is literally meant to move forward and further. And with the energy transition, at Van Bodegraven we aim to use more and more renewable sources. Your energy for tomorrow. We enjoy doing this for and with our customers, suppliers and employees.

Van Bodegraven

Technology used

Other case studies

Showing 9 of 511 items
No more result to load