arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

The Working Principle of a Compression Load Cell

A load cell is a transducer that measures force, and outputs this force as an electrical signal. Most load cells use a strain gauge to detect measurements, but hydraulic and pneumatic load cells are also available.

Strain Gauge Load Cells

Strain gauge load cells usually feature four strain gauges in a Wheatstone bridge configuration, which is an electrical circuit that balances two legs of a bridge circuit. The force being measured deforms the strain gauge in this type of load cell, and the deformation is measured as change in electrical signal. There are several common strain gauge load cell configurations, including shear beam, s-type, and compression.
null

How Does a Compression Load Cell Work?

Essentially, a compression load cell is a block that is designed to hold a load at one point to measure the compression. While tension load cells measure the pulling force, compression load cells measure a pushing force along a single axis. Generally, a compression load cell is placed beneath the object that needs measuring. As mentioned previously, the strain gauge in a compression load cell is deformed when a load is applied, and this deformation is used to produce the measurement. Depending on the application, compression load cells are used to determine any relative changes in resistance. Using the Wheatstone bridge circuit allows these relative changes to be measured with great accuracy, ensuring reliable results. Compression load cells are generally made of materials that are resistant to rusting and scratches, as the base plate should be free from any deformity in order to provide precise results. A hardened cover is often used on the base plate to ensure this. 
Compression load cells are specifically designed for application where space is limited, and they can be built to be extremely compact. They are also ideal for use for extremely high capacity loads – the compression load cells from HBM are available with maximum capacities of up to 50 tons. These load cells are highly accurate, which is useful in industries where products are sold by weight. Many compression load cells are single point, which are extremely versatile and are able to measure off-centre loads, which is helpful for ensuring accuracy. Compression load cells also offer long-term stability, and this stability and accuracy can be further ensured with regular load cell calibration services offered by companies such as HBM. The ease of measurement with a compression load cell helps to speed up processing and output, reducing the time spent obtaining results and ultimately lowering costs.

Compression Load Cells from HBM

HBM supply a selection of compression load cells, that are especially suited for use in process weighing, plant engineering, and tank weighing. We can supply these load cells with maximum measurement capacities from 50 kg to 5 tons, and accuracies of up to 0.1%. We have approvals available for compression load cell installation in scales that are used in potentially explosive environments, or are subject to weights and measures legislation. International certificates for use are also available. If you would like any more information about compression load cells, please contact us and a member of our team would be happy to provide support.

Related Products

No more result to load