HBM Load Cells Provide Accurate Weight Date of the Soil During Subway Construction
Images from the construction site
Issues in Subway Construction
In subway construction projects, the probability of a surface subsidence accident is quite high. For instance, in the construction of Shenzhen subway line 1, the surface subsidence accidents made up for 25% of the total accidents during the total construction period. The accident happened in the downtown area of Shenzhen, which caused serious impact on the nearby buildings and underground pipelines, and also had an impact on the construction progress and raised the cost of the project. Therefore, it is very important to pay attention to how to control the surface subsidence from process schedule of project and cost from the safety side.
As the capital of Guangxi Zhuang Autonomous Region, Nanning is also currently involved in subway projects. Nanning Railway Transportation Group Co., LTD. has asked the Professors from Tongji University to provide a comprehensive solution to monitor the surface subsidence by calculating the volume of excavated soil from the shield tunneling machine.
After very thorough research, the Professors concluded that to control the surface subsidence, the weight of excavated soil must be monitored in real time. HBM, as the leader company of weighing technology will provide the necessary support to the customer on designing the equipment as well as on analyzing the dates.
So as to provide an accurate weight date of the soil, HBM suggested a very classical sensor - RTN.
RTN ring torsion load cells are available with extremely high maximum capacities, and offer an unrivaled precision. During the project Sense Scale & System, who specialize in designing and producing customized weighing equipment, partnered with HBM to offer a comprehensive solution including how to flawlessly connect the loading vehicle at the construction site and transmit the weight signal wirelessly.
The Chinese team of HBM also created software to make it easier for customers to receive and examine the weight data. With the aim of keeping RTN working well for a long time, Sense developed a buffer device and a cross-tie to protect the service life of the load cell.
So as to guarantee the validity of incoming data, Sense selected
AD103C and AED9101 from HBM to guarantee the authenticity of the data, and achieved wireless transmission by RS485 to Wi-Fi module.
The Chinese team of HBM totally understood the demands from customer and customized a software for data collection which significantly minimized the workload of the customer. Through robust technology, products with superior quality, high quality service and reasonable prices from HBM, a traditional weighing system became a very crucial part in Subway construction and won customers’ praise and trust.