Configure
- Immediately ready for use – without any programming
- Sensor database ensures easy setup
- Configure channels individually, in groups, or by EXCEL import
- Password protection of sensitive settings
Aquisição de dados de alta velocidade | Perception
The Perception software is designed for fast and reliable processing of large amounts of data and is therefore ideal for high-speed data acquisition. Thanks to the patented StatStream technology Perception enables 10 gigabytes of data to be visualized on your PC in 10 seconds. For your measurement, this means: Reliable storage and flexible real-time display as well as immediate review. You can access saved data even while measurements are running and zoom in on these data. Recording continues in the background.
Another highlight offered by Perception software is absolute operational security. Reliable data storage and using stable software are enormously important, particularly when tests cannot be repeated or are difficult to repeat. A software crash and the resulting data loss would be extremely expensive, for example, in destructive materials testing or aircraft starts. Perception high-speed software has been designed precisely for these requirements and has been subjected to extensive testing.
Perception and Genesis HighSpeed-specific features enable rapid setup times, quick familiarization and therefore the immediate start of your measurements. Watch this video and see for yourself!
Would you like to use Perception software and/or the Genesis HighSpeed system for your own specific needs? No problem! You can integrate them into your specific environment and use them exactly the way you want by selecting one of the many different interfacing options.
Free Viewer | Viewer Enterprise | Free Standard | Advanced | Enterprise | |
---|---|---|---|---|---|
Features: | |||||
True 64-bit support | |||||
Basic Review, Cursor, Report, Export | Single mainframe control | ||||
Multiple mainframe control | Measurement Uncertainty | ||||
Analysis | |||||
Advanced Report | |||||
Advanced Export | |||||
Video Playback | |||||
Multi-Monitor/Workbooks | |||||
Information sheet | |||||
Basic FFT | |||||
Sensor database | |||||
User/definer mode | |||||
Macros | |||||
Application extensions: | CSI (custom software interface) | ||||
STL & HP-HV automated analysis | HV-IA Impulse Analysis | ||||
ePower Testing |
Título / Descrição | Idioma | Produtos | Idioma | Tipos de Conteúdo |
---|---|---|---|---|
Data Sheets | ||||
Perception Video playback - Data Sheet | English | |||
Perception STL - Data Sheet | English | |||
Perception HV-IA impulse analysis - Data Sheet | English | |||
Perception HPHV automated analysis - Data Sheet | English | |||
Perception eDrive option - Data Sheet | English | |||
Perception Basic FFT - Data Sheet | English | |||
Perception Analysis - Data Sheet | English | |||
Perception Advanced exports - Data Sheet | English | |||
Catálogos | ||||
Genesis HighSpeed - 小冊 | Chinese | |||
Genesis HighSpeed - Broschüre | German | |||
Genesis HighSpeed - Brochure | English | |||
Genesis High Speed - Folheto | Portuguese | |||
Manuais de Operação | ||||
Perception Video Playback Option - 操作說明 | Simplified Chinese | |||
Perception Video Playback Option - 取扱説明書 | Japanese | |||
Perception Video Playback Option - User Manual | English | |||
Perception User Keys and Macros – User Manual | English | |||
Perception STL Analysis Option - 操作說明 | Simplified Chinese | |||
Perception STL Analysis Option - 取扱説明書 | Japanese | |||
Perception STL Analysis Option - User Manual | English | |||
Perception Spectral Display Option - 操作說明 | Simplified Chinese | |||
Perception Spectral Display Option - 取扱説明書 | Japanese | |||
Perception Spectral Display Option - User Manual | English | |||
Perception Software de Aquisição de Dados - Manual do Usuário | Portuguese | |||
Perception Sequencer Control Option BE3200 - User Manual | English | |||
Perception Sensor Database Option - User Manual | English | |||
Perception Repoter Option - 操作說明 | Simplified Chinese | |||
Perception Reporter Option - 取扱説明書 | Japanese | |||
Perception Reporter Option - User Manual | English | |||
Perception Option de lecture vidéo Perception - Manuel d'utilisation | French | |||
Perception Option de création de rapports Perception - Manuel d'utilisation | French | |||
Perception Option d'information Perception - Manuel d'utilisation | French | |||
Perception Option d'analyse STL Perception - Manuel d'utilisation | French | |||
Perception Option d'analyse Perception - Manuel d'utilisation | French | |||
Perception Option d'affichage spectral Perception - Manuel d'utilisation | French | |||
Perception Matlab® Remote Control - User Manual | English | |||
Perception Logiciel d'acquisition de données - Manuel d'utilisation | French | |||
Perception Information Option - 操作說明 | Simplified Chinese | |||
Perception Information Option - 取扱説明書 | Japanese | |||
Perception Information Option - User Manual | English | |||
Perception HV Impulse Analysis Option - User Manual | English | |||
Perception HPHV Automated Analysis Option - User Manual | English | |||
Perception eDrive - User Manual | English | |||
Perception Datenerfassungssoftware Version 6.50 - Benutzerhandbuch | German | |||
Perception Data Acquisition Software Version - User Manual | English | |||
Perception Data Acquisition Software - 操作說明 | Simplified Chinese | |||
Perception Data Acquisition Software - 取扱説明書 | Japanese | |||
Perception Data Acquisition Software - 매뉴얼 | Korean | |||
Perception Data Acquisition Software - руководство | Russian | |||
Perception and GEN series: CSI Programming - User Manual
User manual Perception CSI programming | English | |||
Perception Analysis Option - 操作說明 | Simplified Chinese | |||
Perception Analysis Option - 取扱説明書 | Japanese | |||
Perception Analysis Option - User Manual | English | |||
Quick Start Guides | ||||
Perception V8- Quick Start Guide | English | |||
Perception Measurement Uncertainty - Quick Start Guide | English | |||
Perception Harmonic Analysis - Quick Start Guide | English | |||
Perception eDrive - Quick Start Guide | English | |||
Perception eDrive - Kurzanleitung | German | |||
ePower V8 - Quick Start Guide | English | |||
Outros | ||||
Perception User Keys and Macros – Additional Content | English | |||
Software | ||||
Perception Software 64-bit
Perception 8.50 This is a major release of Perception. Due to the fixes in Perception 8.52, please download Perception 8.52 instead of Perception 8.50. New Features: • Continuous Output • RTFDB processing on CAN signal • Harmonic Analysis Display Improvements • Change from relative addressing to absolute addressing NOTE: With this change. The user already using a setup and using the old relative addressing may have to change their setup. Data: 07/2023
|
Versão: 8.50.23184
|
Tamanho: 665 MB
| Multi idiomas | |||
Perception Software 64-bit
Perception 8.60 This is a major release of Perception. Fixes:: Averaging in Spectral Display always Peak hold average In the Perception Spectral display, the averaging was always peak-hold rather than the selected linear or exponential. This issue is fixed such that now the proper averaging is done. Fundamental calculation issue on RT-FDB A problem with cross-board cycle signals used for doing fundamental calculations was solved. Change of conditional Start/Stop time does not work during the recording In Perception it is possible to conditionally start or stop a recording. Up until now it was possible to change the conditions during a recording which might lead to unexpected or undefined situations. In this release it is no longer possible to change conditions during a recording such that the conditions are always well-defined. Graphical problem in Report sheet tables in Perception A problem with columns width when automatically generating a report was solved. User defined display color is not permanent stored User-defined colors are now stored as part of the PC settings. Switching display mode to ReviewSweep does show the full recording instead sweep A problem with switching between Review and ReviewSweep in the time display was solved. Using macro function auto scale active display y-axis is takes only action on first page of the display The macro function auto scale active display y-axis now works on all pages of a display. The format of the displayed value in a marker does not reflect the format set in Properties for the marker A small formatting discrepancy between marker field and the properties of a marker was solved. Suppress overrange drawing does not work as expected Some related issues concerning drawing or suppressing overrange data where solved. Trace marker not connected to trace line A trace marker is now always connected to a trace. Load Settings menu option doesn't load workbench settings completely A problem with incomplete loading of working bench settings was solved. Apply a Thermocouple type C sensor, Perception shows type B A thermocouple type C sensor is now shown as such. Redo an existing Experiment and load existing Experiment data does not include data On opening Perception and selecting 'Redo an existing experiment and load existing experiment data', the data was not always loaded. This problem is solved. Recordings got locked up by Perception When a recording is finished, it is unlocked and can be accessed by other software. Sometimes the recording was not unlocked and this problem is now solved.
No MDF4 file when exporting using automated processing The problem of a missing MDF4 file when exporting using automated processing was solved. Sluggish behavior when loading a virtual workbench In some case, Perception could react in a sluggish manner when loading a virtual workbench. This problem is solved.
NEW Features: Add hardware settings to a recording stored on a mainframe Up until now, when a recording was made by storing all the data directly on the internal disk of each mainframe (as opposed to storing all or some of the data on PC), the hardware settings of each mainframe were not available in the recording. In the new release, it is possible to include the hardware settings of a mainframe in the recording written to the mainframe's internal disk, in order to know exactly how a recording was made. Automatic merge of mainframe data In the GHS/Perception system, it is possible, and sometimes necessary, to store a recording partially or completely on the internal disc of a GHS mainframe. In this release it has been made possible to automatically merge the different parts of a recording into a single recording file on a PC. An additional improvement in this context is that the speed of transferring a recording from a mainframe to the PC was increased by a factor 2. Rework of the Spectral Display including new features such as:
In the Measurement Uncertainty sheet, support for new hardware was added The measurement uncertainty (MU) of a measurement depends on the properties of the used hardware (sensors, acquisition cards, etc.) which should be incorporated in the MU calculations. In the Measurement Uncertainty sheet, support was added for the T12 w-version torque sensor (but not yet for the minimal torque value of 100Nm). Furthermore, support for the GN610B/GN611B acquisition card was added, as well as support for burden resistors to allow for measuring both voltages and currents with those cards. Allow publishing any value on the fieldbuses in case of an invalid signal Since not all external systems can easily handle NaN, it is now possible to select a user-defined value to publish when a signal is not valid. Allow triggering of signals in Live display based on cycles: In the Live display in Perception, signals are often not stable but 'running', just like in an oscilloscope that is not triggered. In the new release, it is possible to trigger signals based on cycle signals. Periodic signals related to a selected cycle signal will then be stable in the Live display. NEW ePower Suite Features:: Using field bus signals, allow easy detection if a setup is in steady-state A setpoint of an eDrive setup (e.g., the efficiency for a certain torque/speed combination), is commonly measured when a system is in steady-state. In the new release, additional RTFDB functions can be instantiated by the ePower suite which, for a number of relevant signals, determine the mean and standard deviation. The user can determine how the samples to determine if mean and standard deviation are selected in terms of a specified number of samples or as a time interval. NEW Features for Hardware:: XCP over Ethernet This is the first major release which will support “XCP Over Ethernet” in our mainframes. This release supports the functionality of “XCP Over Ethernet – Output” which means data from the mainframe (slave) can be read by the master via XCP. In Perception, Real time data -> Publishing , a new column “Publish to XCP over Ethernet” will be available to allow publishing like existing fieldbus. For generating the A2L file, “Save A2L file as…” button is available. Known Limitations for 8.60 release:
Mainframe control via EtherCAT PDO This is the first major release which will allow mainframe control via EtherCAT PDO. On EtherCAT, several communication protocols are available. Up until now, GHS provided Remote Control via EtherCAT CoE (CAN over EtherCAT), but only SDO as the supported mechanism. From this release onwards, PDO will be supported as well. FieldBus Remote Control documentation may be referred for more information on the available commands and how to use them and return code description. Improvements in Perception :: Modernized the look-and-feel of Perception Many of the icons and graphics were updated to give a more modern look-and-feel and to improve usability. Prevent large MatLab/MDF4 export files due to asynchronous signals In the new release, when exporting signals from Perception to Matlab or MDF4, it is now possible to export asynchronous signals as asynchronous signals, or resampled at a lower user-defined sample rate leading to significantly smaller file sizes for those formats. Improve how a user can see and print the hardware settings from a recording Up until now, hardware settings of a recording could be printed by loading a recording as Active, and then selecting Settings. Two additional entries are shown in the Print sub menu to make this easier: 'Settings from active recording...' and ' Settings from current settings...' . Report CAN signal definition errors in Perception: When a wrong definition of the setup of CAN channels is provided, Perception now gives an error message such that the setup can be corrected. Add key-mouse combination for temporarily grouping of cursors: Currently the user has the option to group/ungroup cursors by pushing a button in the menu bar. To improve usability it is now possible to press the Alt-key, drag one of the cursors and the related cursors will move as a group. This works for horizontal, vertical and slope cursors. Improvements for Hardware:: Allow for unsigned/signed 16-bit CAN inputs Next to 32-bit and 64-bit signed and unsigned CAN signals, we now also allow for 16-bit signed and unsigned CAN input signals. Allow integrating asynchronous samples Up until now, the IntegrateGated() function could only handle synchronous signals to be integrated (such as instantaneous electrical power) but not asynchronous signals which are used, for example, to describe the instantaneous mechanical power. From this release, this function can also handle asynchronous signals. Additional CAN sample rates In previous releases, all CAN input signals to a GHS mainframe were sampled at a rate of 100S/s. It is now possible to choose a different sample rate for each CAN recorder. When choosing a higher sample rate, the maximum number of allowed channels is reduced. The constraint is that the sum, over all CAN recorders, of the product of the sample rate and the number of channels should be lower than 100,000. Some feasible examples are as follows:
Data: 01/2024
|
Versão: 8.60
|
Tamanho: 769 MB
| Multi idiomas | |||
Perception Software 64-bit
Perception 8.54 This is a minor release of Perception. Due to the fixes, please download this release instead of Perception 8.52. Various stability and performance enhancements implemented, see release notes for details. NOTE: With this change. The user already using a setup and using the old relative addressing may have to change their setup. Data: 09/2023
|
Versão: 8.54.23248
|
Tamanho: 732 MB
| Multi idiomas | |||
Perception Software 64-bit
Perception 8.52 This is a minor release of Perception. Due to the fixes, please download this release instead of Perception 8.50 Fixes: No special license for RTFDB on CAN inputs: Perception 8.50 requires a special license to allow processing CAN signals in the RTFDB. This feature is free of charge for customers within Perception maintenance, so it licensing is no longer required. CAN bus stopped unexpectedly A problem is solved where the CAN bus stopped unexpectedly. New type of Peak CAN dongle was not accepted Peak provides the USB CAN dongle with different internal chip sets. The updated Peak dongles are now also recognized and can be used. NaN in log file when doing processing When using one of the FDB functions (CycleFundamental) the output may give NaN. This problem is solved. Freeze when duplicating signals for automated recording processing The system is made robust against selecting the same signal multiple times when doing automated recording post-processing. New Features: Continuous Output
RTFDB processing on CAN signal:
Since some RTFDB functions can generate triggers, this also makes it possible to generate triggers based on CAN signals. Harmonic Analysis Display Improvements:
Change from relative addressing to absolute addressing:
NOTE: With this change. The user already using a setup and using the old relative addressing may have to change their setup Data: 07/2023 | Versão: 8.52.23198 | Tamanho: 727 MB | Multi idiomas | |||
Perception Software 64-bit
Perception 8.28 This is an minor release of Perception mainly improving stability, fixing known problems and adding minor new features. This is not shipped out with the hardware but only available via web download. Details about fixed issues and new features can be found in the release notes. Note: Perception includes the instruments firmware for GEN DAQ systems. So there is no separate firmware available for GEN DAQ systems. When you connect to hardware using a new version of Perception, the firmware in the hardware will be upgraded accordingly to the same release level. Data: 07/2022 | Versão: 8.28.22200 | Tamanho: 602 MB | Multi idiomas | |||
Perception COM-RPC
Installer of the RPC COM wrapper and RPC documentation Data: 09/2023 | Versão: 8.54 | Tamanho: 5 MB | Multi idiomas | |||
Hardware Peripheral Update Package
Update HBM approved GEN DAQ hardware peripherals. For example allowing new types of (solid state) drives. Data: 09/2023 | Versão: 8.54.23248 | Tamanho: 6 MB | Multi idiomas | |||
Hardware Peripheral Update Package
Update HBM approved GEN DAQ hardware peripherals. For example allowing new types of (solid state) drives. Data: 07/2022 | Versão: 8.28.22200 | Tamanho: 5 MB | Multi idiomas | |||
GENDAQ API v3
GENDAQ API v3 for Perception V7.40, V7.50 and V7.60 Data: 01/2019 | Tamanho: 6 MB | Multi idiomas | |||
GEN3i/GEN7i Update Package
The GEN3i/GEN7i Cumulative Update Package contains updated drivers for GEN DAQ “i” type mainframes. There is a version 4.1.1975 of the RTS IEEE1588 PTP driver, and the latest GEN hardware drivers needed when upgrading an older, Windows 7 based GEN3i/GEN7i to Windows 10. Data: 11/2018 | Versão: 8 | Tamanho: 130 MB | Multi idiomas | |||
GEN3i/GEN7i Service Installer
Tool to extract the GEN3i/GEN7i Service from the installed version of Perception. After a fresh install of the Windows OS, the GEN3i/GEN7i service is missing and will be installed using this tool. Data: 12/2020 | Versão: 1 | Tamanho: 181 KB | Multi idiomas | |||
Note: Perception feature preview 10 is temporarily unavailable.