arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Advanced Lightning Warning System Protects Spacecraft Launches at Kennedy Space Center

Kennedy Space Center, USA

Introduction

Better reliability during rocket launching

Using HBK transient recorders and digitizers, HBK has designed a lightning monitoring system for Kennedy Space Center in Florida. The system enhances the safety of operations such as the launching of rockets by ensuring that the risk of damage from lightning is minimized. Lightning is a formidable risk to the Kennedy Space Center’s operations as spacecraft are particularly vulnerable to damage from lightning strikes. In July 2009, for example, the space shuttle Endeavour’s launch pad area was struck at least 11 times including strikes to the lightning mast and water tower leading to costly delays before the launch could be completed successfully.

chevron_left
chevron_right

The Kennedy Space Center’s Florida launch location is ideal because Kennedy Space Center is close to the equator. This means that the earth’s rotation effectively gives an extra push during the launch so that less fuel is needed to reach space. Unfortunately, Florida can often be a challenging launch site because it has the highest rate of lightning discharges per kilometer in the USA making it the lightning capital of the country.

To combat the dangers, the Kennedy Space Center required a lightning monitoring system that could work in parallel with a lightning protection system. Both systems had to be effective at every critical point during a spacecraft’s launch program. Spacecraft are initially assembled inside a huge building called the Vehicle Assembly Building. They are then transported to the pad on special heavy duty transporters called Mobile Launcher Platforms where final preparations and mission checks are performed prior to launch.

A spacecraft is vulnerable to lightning strikes from the moment it emerges from the Vehicle Assembly Building until it is finally launched into space. During this time it is important to continuously monitor numerous points both inside and outside the spacecraft to help determine any possible problems that may have occurred due to induced electrical transients from lightning in the area. To achieve this, HBK developed a system that the Kennedy Space Center utilizes to measure induced currents and voltages at some 120 measurement points. By monitoring multiple points it is possible to identify places where high induced currents occur and hence determine where possible damage might have happened.

A number of factors had to be taken into account when developing the lightning monitoring system. Kennedy Space Center has a high average ambient temperature that can often reach in excess of 90 ° (32 °C) while humidity is also very high, meaning that any system had to be very resistant to corrosion and dampness. Another factor was the high risk of damage from shock and vibration that are present during a spacecraft’s launch making it necessary for the system to meet specific standard military specifications.

It was also considered very important that the transmitter’s input power be DC only. This would allow for battery operation, providing complete isolation, when lightning was nearby. However, it was just as equally important to switch in a DC charging circuit via a remotely controlled output switch on the transmitter once the storm had passed to keep the batteries charged to monitor operations continuously.

The solution selected that satisfied all of the Kennedy Space Center’s requirements was HBK’s Genesis HighSpeed with Perception software as this is a high-resolution DAQ system available out of the box that can monitor up to 64 channels in a single mainframe with a 25 MHz bandwidth and is capable of recording at up to 100 MS/s. It is also capable of window triggering from any channel. Equipment at the test point included a 7600 fiber-optic transmitter rated at 100 MS/s with 14-bit resolution and 25 MHz bandwidth.

The transmitters are housed with stainless steel304; the same material used to protect the Gateway Arch in St. Louis, Missouri, as it does not stain or corrode as easily as ordinary stainless steel. Fiber optic cable was selected because of the long lengths needed – up to 12 km – between the many measuring points. HBK’s equipment has a full scale accuracy of 0.1 % at lengths of over 800 m and benefits from automatic cable length correction while preventing cross channel skew.

Real-time display, navigation, analysis and more, with the perception-software from HBK

All of the sample points are synchronized to IRIG (Inter-Range Instrumentation Group) time codes enabling synchronization and data correlation between channels and other Kennedy Space Center operations regardless of the fiber optic cable length.

The fiber-optic transmitters were linked to an HBK 7600 fiber-optic receiver that accepts up to four 7600 transmitters and provides single mode fiber-optic transmission with 900 MS transient memory. This system also ensured that individual measurement points could be isolated and tested separately from the recording system.

By using HBK’s Perception software the lightning monitoring system can provide real-time display, control and analysis along with numerous other options for analyzing and reviewing any captured data. The system enables multi-monitor display and includes advanced reporting features such as synchronized video playback. Perception also integrates with standard Microsoft Office programs such as Word and Excel.

In addition the system utilizes StatStream© display technology allowing the review of Gigabytes of data in seconds. The system can also produce a remotely controlled test signal to enable verification of the signal path and is capable of providing analysis and generating automated reports based on every lightning event that occurs. The lightning protection system uses tall towers to support metal cables which intercept nearby lightning strikes and divert the current away from the launch vehicle. These are attached to a series of metal wires that route electricity away from the craft. In the test area two launch pads are protected.

Launch Pad 39A – which is designed for the next generation of launch vehicles – has one tower located on top of the pad while Launch Pad 39B – has three 594 ft (180 m) high towers to provide protection. Source NASA picture: https://mediaarchive.ksc.nasa.gov/detail.cfm?mediaid=33077

s a NASA contractor, we take great pride in operating the visitor complex providing hospitality services for Kennedy Space Center. From operating the Kennedy Space Center Bus Tour to serving lunch at the Moon Rock Cafe, our goal is to provide stewardship and hospitality in special places dedicated to creating memorable guest experiences as unique as the destination. The visitor complex is completely funded by visitor-generated revenue and no U.S. tax dollars are used to provide visitor access to the historic birthplace of American spaceflight. As a Smithsonian Affiliate, we offer the chance to view artifacts of NASA’s Mercury, Gemini, Apollo and Space Shuttle Programs in the context of exhibits and attractions that tell the NASA story. 

Kennedy Space Center Visitor Complex is registered with the State of Florida as a Seller of Travel Registration No. KO8282730.

The places Delaware North operates, including hotels, resorts, cultural attractions and parks, make countless memories for millions of guests each and every year. We strive to bring rare attention to detail at every property in our care, and for each and every individual we serve. 

“Delaware North” is a reference to Delaware North Companies, Incorporated and its affiliates and subsidiaries, including without limitation Delaware North Companies, Inc. – Boston, Delaware North Companies Gaming & Entertainment, Inc., Delaware North Companies International, Ltd., Delaware North Companies Landmark Holdings, LLC, Delaware North Companies Parks & Resorts, Inc., Delaware North Companies Sportservice, Inc., Delaware North Companies Travel Hospitality Services, Inc., Delaware North Companies (UK) Limited, as well as numerous location-specific operating subsidiaries and affiliates. References to “Delaware North” or we, us, and ours are used to generally describe the operations and functions of the subsidiaries and affiliates of Delaware North Companies, Incorporated.  

Technology used

Other case studies