Upcoming Webinars (European Time)

Railway Pantograph Overhead-Line Monitoring

  Tuesday, June 25, 2019       10:00 AM CEST       online

Continuous monitoring of contact forces and acceleration between pantograph and catenary in regularly operated railway vehicles is the fundament for a modern predictive maintenance approach. For a safe and highly accurate measurement on high voltage levels HBM recommends a purely optical measurement chain. Acquiring optical sensor information in parallel to vehicle bus signals and position sensing (GNSS) allows you to build a graphical map of your infrastructure and its need for maintenance. This webinar shows the complete setup of the solution.

Read more

Higher RPM and Dynamics in Torque Measurements

  Tuesday, June 25, 2019       2:00 PM CEST       online

The gradual change in mobility concepts from the combustion engine to the electric motor has an impact on test bench measurement technology, which will continue to increase in the foreseeable future. In this webinar, we will discuss how to address these challenges.

Read more

Road Load Data Acquisition with CAN FD

  Wednesday, June 26, 2019       10:00 AM CEST       online

In RLDA and vehicle dynamics testing engineers want to see time sync’d data fusion at the end of their test getting a full picture of what’s going on. This combines analog sensors, vehicle bus information, position and movement (GNSS) and camera. Modern vehicles more and more use CAN FD for ECU inter communication. This webinar will explain how to connect to this new and modern vehicle bus in mobile testing.

Read more

Composites - Hints for Strain Gauge Installation

  Thursday, June 27, 2019       10:00 AM CEST       online

Receive practical hints for strain gauge installation of composite materials.

Read more

How to Correctly Install Force Transducers

  Friday, June 28, 2019       10:00 AM CEST       online

Force sensors are a proven measurement tool. To achieve perfect results, a proper installation is of highest importance. In this 30-minute webinar, we will inform you about the most important rules for the correct installation of force transducers.

Read more

Upcoming Webinars (US Time)

Power Analysis on Complex Drives

  Tuesday, June 4, 2019       2:00 PM ET       online

In this webinar, we will introduce a new power analyzer which is designed for complex applications beyond 3-phase or 6-phase power and efficiency measurements.

Read more

In Vehicle Electric Power Measurements

  Tuesday, June 25, 2019       2:00 PM ET       online

This webinar will explain the reasoning behind in vehicle testing, eDrive’s unique features which make mobile testing possible, examples of mobile power data and why it is needed, correlation to existing DAQ systems, and a brief look at mobile control analysis.

Read more

What you need to know about our webinars

  • What is a webinar?
    The word webinar is a combination of web and seminar: A webinar, as the name implies, is an online seminar, presentation, course or - in some cases - discussion, that aims at teaching the attendees something about the webinar topic.
  • How can I attend one of the HBM webinars?
    Choose a webinar from the list. Click on the title to be directed to a subpage with information on the event and a registration button or directly to the registration page in our online webinar center, called WebEx. Follow the instructions to register for the webinar.
  • Which hardware do I need to attend a webinar?
    You need a computer with an internet connection and speakers or a headset to listen to the presentation.
  • What happens if I have technical problems during the webinar?
    No problem: During the webinar, you can address the presenter or the moderator via the Q&A feature. Your problem will be solved instantly.
  • Can I ask questions during the webinar?
    You can use the Q&A feature to ask questions, which will be answered after the presentation.
  • Do I need to pay for HBM webinars?
    No, all our webinars are free.
  • What if I register, but miss the webinar?
    If you cannot attend the webinar, you usually get the chance to watch a recording of the webinar on HBM.com a few days later. If you're registered, you will also receive an email with more information after the webinar.

Webinars on demand

Val: inget filter

Ditt val gav 47 träffar.

Kontakta Här kan du kontakta oss för att få veta mer om vad HBM kan erbjuda dig.