Nominal (rated) displacement

The force transducer is deformed when the force to be measured is applied. The nominal (rated) displacement specifies the deformation at nominal (rated) force. It is an important characteristic because, together with the nominal (rated) force, it determines a transducer's stiffness. The force transducer's stiffness is crucial to its resonance frequency. From the physical point of view it is absolutely permissible to compare a force transducer with a very stiff spring.

Force Measurement Glossary: Characteristics of Force Transducers

Benefit from our practical on-line glossary to look up the most important technical terms in the field of force measurement:

Kontakta Här kan du kontakta oss för att få veta mer om vad HBM kan erbjuda dig.