Temperature coefficient of sensitivity

Strain gage-based sensors show only a minute change in sensitivity resulting from temperature variation. This is due to the fact that the spring element materials' module of elasticity decreases with increasing temperature - equal force results in higher strain and thus a bigger output signal. The strain gages' gage factor (the sensitivity), too, is dependent on temperature.
With many force transducers the sensitivity's resulting dependence on temperature is compensated for and is thus very small. With both creep and error computation, it is essential that the specified value is always related to the current measured value.

About TKC: The gradient of the characteristic curve varies if the temperature changes.

Force Measurement Glossary: Characteristics of Force Transducers

Benefit from our practical on-line glossary to look up the most important technical terms in the field of force measurement:

Kontakta Här kan du kontakta oss för att få veta mer om vad HBM kan erbjuda dig.