Advanced Aircraft Electrical System Testing

Ditt konto på HBM.com

Omedelbar tillgång till alla nedladdningar

***Om du redan har en inloggning för HBMshop kan du använda samma information för att logga in på HBM.com

Advanced Aircraft Electrical System Testing

Making airborne traffic more environmentally friendly by reducing exhaust gas and noise emissions is what drives the creation of electric aircraft. However, before a fully electric airplane has its first takeoff, a lot of tests are needed.

This webinar will explain HBM’s solution for advanced testing and measurement of components and the complete electrical grid of an aircraft.

In this webinar, you will learn:

  • How a scalable data acquisition system with 4 to 10,000 channels will be used for component testing up to full electrical grid certification
  • About the analysis of the data collected from an aircraft's electrical grid, motor and generator
  • How to directly and safely measure high voltages up to 1,000V and currents

This webinar was originally presented on April 19, 2016.

Presenter:

Dirk Eberlein

  • Product and Application Manager for Genesis HighSpeed 
  • Began working for HBM in 1998
  • dirk.eberlein@hbm.com