arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management
null

So how does a … force transducer actually work?

Force transducers based on strain gauges

Method of operation

To explain how a force transducer works, we first have to answer the question: how does a strain gauge (or SG) work? For most common force transducers have strain gauges inside them. Let us digress briefly to take a closer look at strain gauges: They are electrical conductors firmly attached to a film in a meandering pattern. When this film is pulled, it – and the conductors – get longer. When it is contracted, it gets shorter. This results in a change in resistance in the electrical conductors, and on this basis we can determine the strain, for resistance grows when there is strain and diminishes when there is contraction. To produce a force transducer, in addition to strain gauges you also require a spring element – made of steel, for example. The strain gauge – electrical conductors on film, you recall – is bonded securely to this spring element. As the simplest form of spring element, we can picture a steel cylinder that is either elongated or contracted under the impact of force. We will disregard further forces, such as those coming from the side, in this paper. The force acting on the steel produces mechanical stress in the material, leading to strain. And strain can also mean contraction, because from a physics point of view, this is negative strain.
null

In this article, Thomas Kleckers, Product Manager Force Sensors at HBM, explains how a force transducer works.

Download this article as a PDF

"When it is pulled, things don't just get longer, they also get thinner. Poisson's ratio indicates the ratio of transverse to axial strain. We can compare this with a rubber band, which becomes noticeably thinner when it is stretched." – Thomas Kleckers
null
null
null
If the steel cylinder is contracted it gets shorter, but also thicker. When it is pulled lengthwise, it also gets a bit thinner. How thick or thin it gets depends on the basic mass of the steel. It's obvious that if the steel body is very bulky, higher forces are needed to contract it to a given dimension than if it were very thin. This fact is helpful when building force transducers for different purposes: smaller transducers are used for lower nominal forces, larger transducers for higher nominal forces. Here, the nominal force denotes the intended maximum load of the sensor. But let's return to the strain gauge. A force transducer generally contains four SGs, connected in a "ring" in a Wheatstone bridge circuit, which we are not going to explain in any more detail here (learn more about it in the reference book 'An Introduction to Stress Analysis and Transducer Design using Strain Gauges'). What's important is that the SGs are firmly attached to the steel of the transducer, and therefore undergo the same deformations it does. When the steel is deformed, the resistance of the strain gauge changes, as mentioned above. So, the output signal from the bridge circuit provides information on how great this deformation is. From this, we can calculate the force acting on the SG. This is how the force transducer works. From a mathematical point of view, it is interesting to see that the force transducer functions solely on the principle of linear relationships. Hence, the force is proportional to the mechanical stress (σ=small sigma), σ is proportional to the strain. The relative change in resistance is proportional dependent on the strain. Finally, the output signal of the Wheatstone bridge is linearly proportional to the relative change in resistance of the SG.

What is actually the difference between a force transducer and a load cell?

In principle, they both seem really similar: the load cell measures mass or weight, the force transducer measures force (i.e. N, or Newtons). Surely they are almost interchangeable? Simply enter 100 grams of weight for each Newton, and you can turn a force transducer into a load cell! But it's not that simple.

Difference 1:

The load cell measures mass, and only ever in one direction, because the mass is always greater than 0. If a container is placed on a load cell, this cannot suddenly lift itself up and produce a negative weight. The force transducer, on the other hand, measures negative and positive forces, tensile and compressive forces.

Difference 2:

The load cell is produced then installed somewhere or other at the user's plant, then calibrated on site. Force transducers are calibrated at the factory immediately following production, and must always measure the same, even if removed and installed several times. The force transducer therefore has a more robust construction than most load cells, in order to guarantee the reproducibility of the measured values under varying conditions.

Difference 3:

The load cell must satisfy certain legal requirements, regarding legal-for-trade capability, for instance. The force transducer fulfills different regulations – standards, such as VDI 2635 or ISO 376. Unlike the load cell, the above-mentioned reproducibility, for example, is an important factor.
null
null

Fields of application

"Force transducers are used virtually everywhere – it's hard to imagine. I was particularly impressed by one test bench usage whereby a force was measured across an air gap. In other words, measurement is taking place even though the force transducer is not touching the platform. I still find it incredible today that this actually works" – Thomas Kleckers

 

To conclude, we'll take a look at business – a few fields where force transducers are used.

  • Tests on objects test how much force is acting on them. Example: The impact on a motorcycle helmet, as in an accident.
  • Reference measurements are used to produce domestic and international comparability between measured values. Here, metrological institutes around the world use especially precise force transducers to test systems. These institutes then supply reference values for the entire domestic and international economy.
  • On test benches, force transducers often ensure that a desired material load can be precisely controlled: when the wing of an airplane is pushed to and from with the aid of a machine, to simulate real flying conditions, for example.
  • Industrial machines and systems need force transducers for metering forces, e.g. in presses, assembly lines or end-of-line tests. Example: How firmly must the cap of a pen be pressed in order to stay on?

Related Products

No more result to load