arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

A Driver of Innovation for Electric Motors with a Highly Efficient Test Bench

Schabmüller GmbH, Bavaria

Introduction

Together with HBK, Schabmüller has developed a new test-bench for a new type of drive and benefits from precise and cycle-accurate testing equipment.

chevron_left
chevron_right

Highly Efficient Test Bench For e-Motors

Schabmüller GmbH is the market leader in producing electric motors for mobile machinery. Together with HBK, Schabmüller has developed a new test-bench concept for a new type of drive. It combines the advantages of precise and cycle-accurate testing and measuring equipment with those of convenient test-bench development. This concept facilitates easily integrating sensors into the measurement system and controlling tests based on acquired data. Thanks to the formula database, which also provides formulas for real-time DSP calculation, the motor developer can quickly and easily create individual calculations – for customizable measuring and testing tasks.

Electric machines are the drives of today and the future. While the automotive industry still struggles with this transition, electric machines have been the standard in vehicles such as forklift trucks for over 50 years. Moreover, the requirements for motor performance and efficiency are continually rising. Hence, electric motor manufacturers work continuously to develop new drives. Simultaneously, new test-bench concepts are in demand to test these new motors with the required accuracy. The challenge is to obtain reliable results while precisely controlling test processes. Schabmüller GmbH, the world’s largest independent manufacturer of electric motors for battery-powered vehicles, also applies these requirements to its own test equipment. Together with HBK, the electric motor producer has developed a test-bench concept that enables measured data to be acquired and evaluated in line with these requirements. Schabmüller designs electric drives for forklift trucks, hybrid trucks and buses, as well as for construction and agricultural machinery. Schabmüller developers rely on HBK's extensive measurement technology in their new synchronous motor test bench, specifically the Genesis HighSpeed data acquisition system and the Perception software program.

A software program developed using National Instruments’ LabVIEW* development environment is deployed for automating and controlling the test bench. "The Genesis HighSpeed measurement system is exceptionally easy to work with and all processes run in parallel and in real time. This makes the development processes of our test bench software much easier and less complex," explains Dr. Martin Hafner, Manager of Technology Development for Permanent Magnet Synchronous Machines at Schabmüller. "Personnel expenses are considerably lower with Genesis HighSpeed in comparison to a measurement system based on National Instruments components alone."

A modern test bench concept for innovative electric motors

As a driver of innovation in the industry, Schabmüller now also offers its customers permanent magnet synchronous electric motors. This new type of drive, without any changes to the cooling concept, produces just as much power as comparable asynchronous motors while requiring considerably less space. Optimizing or revising the cooling concept enables this effect to be disproportionately increased. To achieve this, synchronous motors must meet high requirements, be powerful and energy-efficient, and have a high energy conversion efficiency to optimally use the supplied energy. To ensure precise tests for the new electric drives, Schabmüller worked with HBK experts to optimize the test bench’s entire measurement chain.

"We chose the combination of Genesis HighSpeed and Perception software, as well as the LabVIEW development environment because Perception and LabVIEW are very easy to connect with an interface,"

according to Stefan Lauck, development engineer at Schabmüller. "Thanks to the Perception sensor database, we can also integrate a wide range of different sensors for current, voltage and torque into the measuring system quite easily, simply by plug-and-play, like inserting a USB device in a computer. Integrating vibration sensors as part of electrical measurement equipment is possible without any problems. That saves us time and resources in setting up the test bench."

The Schabmüller test bench is used for various measurement tasks to reliably determine the short-term or continuous power and energy conversion efficiency of synchronous machines, or to identify their service life and component reliability. Schabmüller experts measure rotational speed and torque, generate efficiency maps, and, based on this measured data, determine longitudinal and transverse inductances. Additionally, Schabmüller implements service life experiments under maximum mechanical stress. Long-term thermal experiments also determine how various long-term and interval loading patterns affect the motor function. "The electric motors have to achieve a service life of at least 50,000 hours," explains Stefan Lauck.

INTERNAL USE - Case Study  schabmuller test-bench-edrive2

Optimized measurement chain: Schabmüller worked with HBK experts to develop a new test-bench concept. The combination of HBK’s Genesis HighSpeed data acquisition system and Perception software with the LabVIEW development environment allows precise measurements alongside convenient and fast analysis.

INTERNAL USE - Case Study  schabmuller test-bench-torque-transducer2

Demanding measurement tasks: In Schabmüller’s test bench, torque transducers measure the torque and transmit the results to HBk’s GN610B and GN1610B data acquisition cards that record the measured data with high-resolution sample rates of up to 2 MS/s.

INTERNAL USE - Case Study  schabmuller screen-labview-perception2

Absolutely synchronous: HBK’s Perception software communicates with the LabVIEW development environment via a freely programmable software interface.

An optimum system for extremely fast real-time tests

To securely and reliably determine all measured data, the test bench’s individual components must work together perfectly. The sensors acquire measurement signals such as current, voltage, temperature and torque and forward them to the data acquisition system. The Genesis HighSpeed GEN7tA data acquisition system is used on the Schabmüller test bench along with GN610B acquisition cards. The DSPs, digital signal processors on the cards, process the measured data and calculate the initial results in real-time. The calculated measurement results are forwarded to LabVIEW for analysis – at up to 1000 times per second thanks to the EtherCAT connection. In parallel, HBK’s Perception software also saves all the acquired raw data. "Measured data and real-time computing results are acquired and forwarded simultaneously and with the same time stamp. That's an enormous advantage for analysis," emphasizes Stefan Lauck.

"We can also create our own formulas for the calculations in Perception and save them in the formula database. These formulas can be used in both post-process and real-time calculations in the DSPs, without any programming of the respective computer architecture.”

Perception communicates with the LabVIEW software via a freely programmable software interface. The LabVIEW software is responsible for controlling and automating the test-bench processes. Based on real-time computing results, it controls the load and test specimen machines’ inverters. "The measured data can be processed for cycle-synchronous individual values. Then only the relevant cycle-synchronous computing results are used for control and automation of the test processes. For example, the RMS values of current and voltage or the torque values," says Stefan Lauck. "Since, if need be, the raw data will still be saved, we can also use it for more extensive post-process analyses." In addition to the cycle-synchronous individual values, continuously measured data can also be linked in the Perception formula database and processed in real time. No programming knowledge is required for this either.

Easy sensor integration and channel synchronization

"The combination of LabVIEW and HBK's Perception software really does offer us many advantages," says Stefan Lauck. "Genesis HighSpeed synchronously records measured data of sensors and allows for sample rates of up to 2 MS/s on up to 51 power channels. It automatically synchronizes the sample rates of the different channels and input cards. This considerably reduces users’ overhead. We were also able to make optimum use of LabVIEW advantages, such as the TDMS data format, to rapidly save large amounts of data. This also facilitates the subsequent data analysis using a wide range of available software products."

Schabmüller’s developers received customized support from HBK’s Perception experts as they integrated the data acquisition system into the test bench. According to Stefan Lauck: "Perception is an efficient software program that acquires data reliably. Thanks to the introductory training from HBK, we quickly became proficient. And because Perception is so easy to work with, we are able to define measurement sequences for our specific purposes."

Thanks to the Perception sensor database, a wide range of different sensors can be integrated into the measurement system simply by plug-and-play. Genesis HighSpeed reliably acquires measured data, calculates measurement results in real time, and makes them available for test-bench control. User-defined calculation formulas can be created without any programming knowledge and can also be applied to measured values in real time and to saved data in post process. This results in more efficient test processes with lower personnel expenses.

 

* LabVIEW is a trademark of National Instruments. Neither HBK, nor any software programs or other goods or services offered by HBK, are affiliated with, endorsed by, or sponsored by National Instruments.

About Schabmüller GmbH

Schabmüller GmbH is the world’s largest independent manufacturer of electric motors, producing more than 300,000 drives per year and having annual sales of over 90 million euros. The company from Berching, Bavaria, has been a supplier for international producers of forklift trucks, construction and agricultural machinery, as well as hybrid buses and trucks for over 50 years. For its range of forklift trucks, Schabmüller produces DC, asynchronous, and synchronous motors that are deployed as drives in propulsion and steering systems or pump motors for the mapping of lifting processes in these vehicles. One reason for the company's success – Schabmüller does not develop any standard motors, but instead, focuses on developing customer-specific and tailor-made motors for specific applications.
Stefan Lauck

Technology used

Other case studies

Showing 9 of 511 items
No more result to load