Shock Testing
- Rocket Engine Tests
- Ballistic Tests
採用Genesis High Speed進行振動,衝擊測試
There are different kinds of shock tests, vibration tests or impact tests, for example, rocket engine tests, blast and explosive measurements, Split Hopkinson bar material tests, Charpy tests, bird strike or general component crash tests. What they all have in common is that they reproduce extreme events. For when a product or test sample is subjected to extreme, sometimes even ballistic shock testing the test runs involved need to be perfect. Especially with shock tests, the test setups are expensive and often cannot be reproduced at reasonable expense.
HBM's Genesis HighSpeed DAQ system provides a solution that has been tried and tested in shock, vibration and impact tests in the market for many decades. Genesis HighSpeed* knows the "number one measurement quantity" for these tests is reliability.
Thanks to perfect interaction with the integrated Perception software, Genesis HighSpeed guarantees absolute data security, plus an extremely high sample rate of up to 100 MS/s that allows deep insights into the test objects even during the shock and other events. Plus: The incoming measurement data can be visualized virtually in real time using the patented StatStream technology, and the Review-while-Recording function provides an overview of all the data of the ongoing recording.
Image above courtesy of ATK.

Scalable and flexible data acquisition systems with 4 to 10,000 channels

Different types of input cards with sample rates up to 100 MS/s supporting various sensor types

Local storage options for highest data security

Perception software for setup of the data acquisition system – no matter if it has 4 or 10,000 channels
Every shock testing, impact testing and vibration testing application has its own challenges. Many of our customers master these challenges using the Genesis HighSpeed data acquisition system. The system consists of different mainframes and data acquisition cards and offers the following:
* HBM Genesis HighSpeed products were previously marketed under the LDS Nicolet, LDS Dactron and Gould Nicolet brands. The Nicolet brand is owned by Thermo Fisher Scientific Inc. Corporation. Gould is a brand of Gould Electronics GmbH.