The Hardware: Torque, Power Analyzer, and Splitter Box
In the test rig used to demonstrate an electric motor test, we are using a torque transducer which is placed between the drive and the brake. With this test rig, we can control torque and speed to look at the different output states to imitate real world scenarios. The output of the torque and speed sensors are connected to our eDrive power analyzer which time aligns them with the voltage and the current signals.
You also have the option to add other channels to measure temperature or vibration. The power analyzer can be connected to either a PC or a tablet for setup and data analysis in the eDrive software. The system could also be set up using software commands by utilizing our API. The splitter box connects the torque and speed outputs to the power analyzer and provides the possibility to repeat the signals for your automation system.