arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

HBK Measurement Technology Optimises a Vehicle's Wishbone

highspeed karlsruhe, germany

Introduction

In the international "Formula Student" competition, teams from colleges and universities compete against each other in a wide variety of disciplines with vehicles they have designed and built themselves.

One of the teams is "High Speed Karlsruhe" from the Karlsruhe University of Applied Sciences, which is constantly searching for new ways to achieve the fastest possible lap time.

chevron_left
chevron_right

To achieve the best possible lap time, low weight is crucial for High Speed Karlsruhe's vehicle. This can be achieved by reducing the undamped masses, including the weight of the wishbones. 

The idea is to manufacture the wishbones entirely from carbon fibre-reinforced plastic. Therefore, simulations were carried out to analyse the effects on the wishbone, which now have to be validated with physical tensile and compression tests. 

The Idea: A Wishbone Made of Carbon Fibre-Reinforced Plastics

To reduce the weight of the vehicle, the undamped masses located between the tires and the spring/damper package must be reduced first and foremost. This also includes the wishbones, which connect the steering knuckle to the chassis. To reduce their weight the wishbones were entirely manufactured from carbon fibre-reinforced plastic. Thanks to the new wishbones, the following benefits can be achieved:

  • Lower weight
  • Control through in-house production
  • Higher stability

In order to exploit the benefits, the action on the wishbones must be analysed in detail, for which simulations are carried out in advance. To verify these simulations, tests must be carried out with bonded strain gauges to determine how the actual forces correspond to the results of the simulation.

INTERNAL USE - Case study optimized Wishbones for reduced lap time
INTERNAL USE - Case study optimized Wishbones for reduced lap time

High Speed Karlsruhe, Vehicle F-117

HBK strain gauges are bonded to the surface to determine how the actual forces correspond to the results of the simulation. Moreover, the results provide a basis for further vehicle tests and the design of future wishbones.

Preparation of the Measurement: Simple Installation of Strain Gauges with the HBK Starter Kit

For tensile testing on a test rig, the control arms of the vehicle must be prepared. To optimally record the forces, strain gauges must be installed in the direction of force application along the wishbones. This is done by using the HBK Starter-Kit, which contains all the necessary materials for the installation.

To install the strain gauges correctly, the surface must first be cleaned with a chemically pure cleaning agent (e.g. RMS1), which is included in the starter kit. Cleaning is easy using the enclosed non-woven pads. Subsequently, the surface is roughened in several passes with sandpaper and cleaned again with the enclosed RMS1. The strain gauge is installed on the wishbone using the fast-curing Z70 adhesive and the integrated fluoropolymer release film. 

INTERNAL USE - Case Study  high-speed-karlsruhe case_stud_optimizing_vehicle_wishbone_resource_345px

Measurement Setup and Execution of the Measurement

The tensile and compression tests are carried out in the laboratories of the Karlsruhe University of Applied Sciences to test the material connection of the strain gauges to the carbon fibre-reinforced plastic tube and to evaluate whether future tests would work on the moving vehicle. 

For this purpose, the control arms are clamped in the testing machine. This is done using a specially designed and manufactured clamping device, which optimally fixes the control arm. 

The voltage output of the HBK analogue amplifiers is measured with a multimeter and then compared with the results of the tensile testing machine. 

Since only one of the two struts is used for the measurement at a time, the second strain gauge is used for thermal compensation with a quarter-bridge circuit. For this purpose, the settings of the values for the strain gauges, which can be found on the enclosed data sheets, are entered into the measuring amplifier and adjusted with an integrated rotary potentiometer.

INTERNAL USE - Case Study  high-speed-karlsruhe case_stud_optimizing_vehicle_wishbone_result_traction

The Measurement Results and Their Interpretation

The measurement was carried out according to the principle of linearization to enable different forces to be applied by the testing machine and the stresses to be read off at these points. This makes it possible to determine whether the strain gauges show an identical force curve as, in this case, the tractor.

INTERNAL USE - Case Study  high-speed-karlsruhe Bild8

About High Speed Karlsruhe

For 10 years now, the "High Speed Karlsruhe" project of the Karlsruhe University of Applied Sciences has been participating in the Formula Student competition with specially developed and manufactured vehicles. 

The Formula Student offers students of technology and economy the possibility to convert theoretical knowledge into realistic practical experience. The goal is the independent development, construction and production of a racing car by the student teams over one year. Currently, 44 students from a wide variety of courses and alumni of Karlsruhe University of Applied Sciences are working together on the development and production of vehicles.

More about High Speed Karlsruhe


Technology used