arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Aqira - Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All Aqira See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Rainpower Uses HBK Equipment to Develop a Unique Flight Recorder Tool for Accurate Dynamic Measurements on Water Turbines in Hydropower Plants

Rainpower as, norway

Measurements on Water Turbines

Rainpower AS provides professional engineering services for the development of hydroelectric power. Based in Trondheim, Norway, the company’s turbine lab has played a pivotal role in testing and developing new turbines since 1985 and has been involved in some of the largest and most prestigious projects in the world, such as the Three Gorges Dam project on the Yangtze River in China.

chevron_left
chevron_right

When it comes to water turbines, runner blades are a critical component. Often faced with tough conditions, such as high-water pressure and water speed, it is important to ensure specifications are consistent with the performance of the blade.  

To address this issue, Rainpower have developed a new measurement tool called a Flight Recorder to accurately measure the dynamic stress on runner blades during all modes of operation. HBK was invited to step in and specify a solution for the Data Acquisition System (DAQ) part of the unit.

The Flight Recorder is a battery-operated system, where all data is stored locally, negating the need for an underwater data transmission system. Used to measure strain on turbine blades, pressure distribution in the runner in different places, vibration on different locations, and temperature on the runner surface, such data is invaluable for calibration of data simulations and numerical analysis.

null

Meeting the Need

For this project, QuantumX units from HBK were used to collect data with a CX22 industrial computer/data recorder, with flash memory. The system, which runs with catman software, was mounted in a tailor-made framing system, and placed inside waterproof housing with waterproof subsea connectors.

The QuantumX data acquisition system (DAQ) is the perfect tool for reliable data acquisition of different physical quantities and sensor technologies. Flexible, reliable, and easy to use, the system is small and portable, meeting the design requirements specified. 

Before testing, HBM strain gauges are applied to runner blades on predefined spots, and the other transducers are mounted on their appropriate places. All transducers are then connected to the Flight Recorder with watertight cables, and the unit is then mounted onto the hub of the runner. Before filling the turbine with water, the recorder is switched on and the catman program starts collecting data. The recorder then collects data during filling up the turbine, through different modes of operation, after shutting down and when the dewatering of the turbine starts. When the system is empty, the runner can be inspected, and all data from the Flight Recorder can be transferred to a laptop, and a brief check of the collected data is done. Back in the office the measurement data can be conveniently analysed with advanced algorithms.

This is particularly important as it enables Rainpower to provide customers with accurate and valuable information on how parameters such as the number of starts, stops and operation in different power ranges can affect the lifetime of the runner.

“As a company dedicated to testing, we needed to choose the right equipment for this project. So, following a market review, we opted to use HBM components. HBM provided us with excellent service and knowledge in the strain gauge market, which was an especially important aspect to us”,

explains Kjell Sivertsen, Discipline Manager Lab Technology and Equipment, Rainpower AS, Turbine Laboratory, Trondheim.

With the development of the Flight Recorder proving such a success, Rainpower AS hopes to undertake a further three to four tests later this year, both in Norway and Sweden.

As renewable energy sources continue to play an increasingly important role in the energy supply worldwide, HBK was delighted to be able to assist Rainpower AS on this project. Furthermore, as Rainpower AS continues to put more and more emphasis on the development of new turbines, HBK looks forward to continuing this relationship in the future.

Rainpower AS is a Norwegian company that develops, designs, manufactures and markets equipment for hydropower generation. Rainpower has more than 165 years of experience in the hydropower industry. With the help of HBK's equipment and experience, the company has been able to solve their problems in data acquisition of different physical quantities and sensor technologies.

null
null

Related Products

No more result to load