arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Green energy production: Increasing the future service life of fermentation plants through "on-site" measurement technology.

Axpo Kompogas AG, Switzerland

Introduction

Axpo Kompogas AG produces energy and bio fertilizers from organic waste in more the 75 fermentation plants around the world. In order to improve the service life of its biogas plants, the Swiss company has decided to use a measurement technology solution from HBK. But how can sensors be securely and permanently installed in the wet and aggressive environment of a fermenter? The solution was offered by a process that HBK developed for offshore applications in the open sea.From the waste resource economy: This is the gold standard for sustainable success in an era of increasing environmental and efficiency awareness. An important role in this concept is played by fermentation plants that produce biogas - and therefore , usable energy - from organic waste such as leftover food or garden compost. With more than 20 years experience in this sector and over 75 plants in operation around the world, the Swiss company Axpo Kompogas is one of the leading operators and project developments in this branch. Axpo Kompogas operates 16 fermentation plants itself in Switzerland. The company manages a further nine plants with partner companies. These plants fermented more than 184,000 tons of bio waste in total during 2010. The net power production amounted to 22 million kilowatt hours.

chevron_left
chevron_right

Increasing the service life of fermenting plants.

Continuously rotating paddles are used in the fermentation plants to circulate the biomass. In order to optimize the service life of their plants and obtain detailed information about possible deformation of the paddles, Axpo Kompogas decided to install a comprehensive measurement technology monitoring solution from HBK in their fermentation plant in the Swiss town of Chavornay, in the canton of Waadt. The Axpo Kompogas engineers also hoped to obtain more in-depth knowledge about the various forces acting on the plant equipment.

Installation of strain gauges directly on the stirrer

The strain gauges applied directly to the stirrer paddles will detect loads, overloads and deformations. This means the measurement technology is really "on site" and directly where the action is. This allows previously implemented calculations and simulation to be verified, and to indicate and implement constructive improvements for future plants based on the actual occurring forces. However, the ambient conditions in the fermenter pose a particular challenge for the installation of the strain gauges. The paddles, and therefore the measurement points for the strain gauges and relevant cables, are located directly in the biomass, a constantly wet and aggressive environment. This means: the measurement point and cable must be absolutely resistant against biomass and moisture.

Because of this difficult task, Axpo Kompogas decided on a complete HBK solution: Strain gauges, a measurement data aquisition system and evaluation software - together with the direct installation of the measurement technology on site by experienced HBK service technicians.

The HBK experts installed the strain gauges directly to the stirrer paddles and ensured the measurement points were professionally and permanently protected by means of a special multiple seal. In this case, they used the HBK know-how, unique worldwide, acquired during the installation of strain gauges in wind energy offshore plants, where the measurement technology needed to be installed and appropriately sealed in locations up to 30 meters under seawater.

Measuring amplifier systems SoMat eDAQlite

The "HBK SoMat eDAQlite" amplifier in use here, which is applied directly to the face of the shaft, can also display all its particular strengths. SoMat eDAQlite is not only small, it can also be used under extreme ambient conditions. The processed measured data is stored in eDAQlite and (if required) compressed, and can be read in the HBK evaluation software catman® on the PC when necessary via the Ethernet interface. The Axpo Kompogas technicians have access at all times to the measurement data with this monitoring solution.

It was important for Axpo Kompogas to have HBK as a partner for the complete measurement technology solution. With this complete solution, Axpo Kompogas was able to put an operational measurement system into operation - with minimum training requirements and perfectly designed for the hard conditions of the fermenter. HBK took over the responsibility for the entire measurement chain project and ensured scheduled completion by the time the fermenter passed acceptance.

Security through early damage detection

Security through early damage detection - an advantage not only for Axpo Kompogas. Such monitoring systems offer solid economic advantages in numerous applications. With this complete solution, HBK offers "turnkey" solutions, even down to complete installation on request for extreme application conditions.

AXPO

Axpo is driven by a single purpose – to enable a sustainable future through innovative energy solutions. Axpo is Switzerland's largest producer of renewable energy and an international leader in energy trading and the marketing of solar and wind power. Axpo combines the experience and expertise of more than 6,000 employees who are driven by a passion for innovation, collaboration and impactful change. Using cutting-edge technologies, Axpo innovates to meet the evolving needs of its customers in over 30 countries across Europe, North America and Asia.

More about AXPO

Technology used