arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

CLES-FACIL: Research of Safe Parachute Opening

cles-facil, France

Introduction

Every year a team from the aeronautical association "CLES-FACIL" develops an experimental Rocket in order to research key scientific questions. In a project to calculate the force that is exerted upon a rocket through the opening of a parachute, "CLES-FACIL" uses HBM strain gauges.

Not all questions about air and space travel have been explained. Therefore Institutions worldwide have conducted many projects with the aim to research further into areas that are scientifically questioned. In 1967, Alain Juge founded the club Lyonnais d'Experimentation Spatiales (CLES-FACIL), the oldest aeronautical research association in France. A strong connection between the club and the well renowned INSA University in Lyon means that research projects are continually carried out at a high level.

chevron_left
chevron_right

Detrona Project: Measuring the force from a parachute

The task of the 2011 rocket "Detrona" from CLES-FACIL was, amongst other things, to find out the force that the opening of a parachute exerts on a rocket. This value before now was only ever formally calculated and never actually measured. Therefore the exact knowledge of this value is of great importance to Rocket makers because: The opening of a parachute causes a "shock" to the Rocket, which, in this case, could cause irreparable damage to the complete Rocket construction.

The Fusex Detrona is just short of 2 meters in length, with a diameter of 120mm and a weight of 10Kg. Parts of the rocket are transparent Polycarbonate in order for the installation of an on board camera to shoot 360°. In addition to this, a parachute is mounted, from which the force measurement will be taken.

Semi-analytical Force Measurement

Altogether the force, upon the opening of a parachute, can be estimated through a semi-analytical formula: F=0,65*S*V2, whereby S represents the surface area of the parachute and V is the speed at the moment of opening. The speed of V can not be estimated and the size of the parachutes surface area really depends on the form that it opens in. Therefore the Team from CLES-FACIL decided to use HBM Strain Gauges to calculate the force of the Rocket Detrona.

The Strain Gauges were installed on the Parachute mounting in opposing directions, two in the direction of tension and two in the direction of compression. This layout allows Torsion and Strain flows to be blended out. In addition, there is an amplifier and a form of calculating software to record the measurement data.

Application of Strain Gauges on the Parachute mounting of the Detrona

Successful test flight and acquirement of measurement data

The test flight, within which the Detrona Rocket was equipped with the strain gauges and telemetric system, was very successful. The Rocket reached a height of over 1000 meters. The opening of the parachute proved reliable and precise. Through the telemetric system the team collected all the relevant measurement data, and showed that the maximal force, which was exerted at the opening of the parachute, was 1210 Newtons.

The graph shows the development of force, which was measured during the Rocket flight. The different stages from the start of the flight to the expansion of the parachute are clearly identifiable.

The measured value from the flight helped the CLES-FACIL team in further developments and was also recognised in the field of aerospace. So much so that, due to the project Detrona, the CLES-FACIL won the first prize in the 2011 "Planète Sciences" C'Space competition for the third time. Moreover, a further prize was won the "Thalès Alenia Space" hosted by the French Air and Space-Travel association GIFAS.

Click here for reports of the Detrona project (In French)

The Customer

CLES-FACIL

Watch a video on the Detrona Project

Follow up projects with Strain Gauges
Further measurement technology projects are already in place. As a follow up project from Detrona, is the investigation into Stress Analysis of an Aileron on a rocket. Here again the team will use Strain Gauges from HBM.

HBM Strain Gauges

Strain Gauges