arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

UPC: Tests for externally reinforced concrete beams

universitat politècnica de catalunya, spain

Introduction

The structural research team at the Universitat Politècnica de Catalunya (UPC), Barcelona, Spain, has developed tests to determine the stresses in concrete beams that are used in construction.

chevron_left
chevron_right

The structural research team at the Universitat Politècnica de Catalunya (UPC), Barcelona, Spain, has developed tests to determine the stresses in concrete beams that are used in construction. The tests, that have taken the past two years to develop, focus on the use of externally reinforced carbon fiber laminate to reinforce the concrete beams. The use of carbon fiber laminates (CFRP) has increased over the past several years. CFRP characteristically has its fibers running in one direction to provide a semi-rigid structure with high modulus when bonded with an epoxy adhesive. The laboratory tests were undertaken to simulate various types of failures that can commonly occur. These include:

  • Removal of a concrete roof
  • Removal of the end laminate interfacial
  • Detachment of the laminate interfacial induced by the fracture
  • Shear failure in concrete

Tests with 24 strain gages

The tests undertaken by the Laboratori per a la Innovació Tecnològica d'Estructures i Materials (LITEM) involved fitting the beams with 24strain gages of type 1-LY41-6/350. These were pasted in position using HBM adhesive X280. Strain gages were placed under the beam and along the CFRP strips with two at each side on position L/4 for linear displacement. In addition two laser sensors were placed – one on either side at the center of the beam – for triangulation displacement measurements.

Signal capturing with MGCplus

The signals were captured using HBM’s MGCplus with three AP815i modules for the strain gages while an AP801 module was used for the laser sensors. Load and displacement signals were detected by a 250 kN actuator. HBM’s catman®APdata acquisition software was used to analyze the results. Traditional beam theory was used to calculate the reinforced beam bending forces and these were subsequently compared with the data obtained from the tests. This enabled the general equation for doubly-reinforced concrete beams and beams reinforced with external laminates such as fiber-reinforced polymers to be modified to give more accurate estimations for deformationεdb (deformation blast-off). Future tests may also utilize gages attached to the laminated embedded on the tension face of beams.

More information about BarcelonaTech University

Related Products

No more result to load