arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Aqira - Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Veneta Engineering: Height measurement tests

Veneta Engineering, Italy

Introduction

The Ponte della Costituzione is designed by the Spanish architect Santiago Calatrava and became the fourth bridge over the Grand Canal in Venice when it was inaugurated in September 2008. HBK Italy worked with Verona-based Veneta Engineering which was in charge of all optical height measurement and trigonometric leveling tests on the bridge, as well as determining the deformation and stress states needed for the acceptance inspection of the bridge in November 2007.

chevron_left
chevron_right

Load testing on the Ponte della Costituzione in Venice

Veneta Engineering in Verona is one of the most important test and inspection companies in Italy for safety checks and European acceptance inspections.

The company has been working in this field for more than 20 years and is highly regarded for the reliability and quality of its work.

The main structure that needed testing was designed as an arched truss comprising six cuboids over a total length of about 81 m. The load tests were performed with the bridge on its support pillars, without any temporary bridge abutments in the river bed and secured with lightly reinforced concrete. 

Four hydraulic pulling-lifting blocks were used, each with a mechanical load of 120 kN, as well as four tanks of 3.55 m x 15.85 m x 1.20 m, which were filled with 260 m3 of water in the central part of the bridge.

Stress analysis during the construction phase

Measurements were taken between ribs R14 and R14’ with an evenly distributed loading and at ribs R22 and R22’ with selective loading.

This checked the actual longitudinal and transverse deformation of the bridge. The conformity between the computer model and the construction was also checked to verify the structure’s effective rigidity.

To capture the data around forty XY71-3/120 strain gages were installed with two measuring grids offset by 90°. The adhesive used was two-component X60 adhesive with a composite material with an aluminum layer, ABM 75, acting as the covering agent.

Because of the length of the bridge, the measuring points were connected in a 6-wire circuit, which excluded measurement error as a result of voltage loss in the cables.

The MGCplus amplifier system with ML801 and AP815i modules were also used. Because of the high atmospheric humidity, the biggest challenge was choosing the right adhesives and protective materials, as well as laying the cables.

The data was recorded for about a week by catman®Professional software and delivered excellent results.

Company

Veneta Engineering Srl was founded in 1980 with the aim of establishing a point of reference for engineering activities in the area.

Always projected towards the cutting edge and innovation, Veneta Engineering Srl immediately aimed at the idea that even in Italy it was necessary to achieve a modern and effective operating method for quality control , although the time was not yet entirely ripe for the production fabric of the time.

However, foresight has borne fruit over the years, with new perspectives that have become increasingly interesting. A real turning point was marked with some large contracts:

  • the works related to the Italia 90 World Cup
  • the third motorway lane (Bs-Pd)
  • the works of the "Quadrante Europa" district of the city of Verona

Technology used

Other case studies