arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All Aqira - Test Data Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Medellín Metro: Portable diagnosis system for mobile data acquisition

EAFIT University, Colombia

Introduction

A major project being run by the EAFIT University – Colombian Institute for the Development of Science and Technology (Colciencias) and the Medellín Metro analyzed the dynamic response of the passenger cars.

chevron_left
chevron_right

The two organizations needed to examine the operating conditions of the metro in Medellín to ensure it conformed with international railroad standard UIC- 518. This contains all the details for testing the ride performance of rolling stock from their dynamic response, in order to assess safety, track stress and ride conditions (stability, comfort, etc.).

Position and mounting of the force and acceleration transducers HBK‘s U2B/100 force transducers were selected for mounting on the car axles of the train. The B12/500 acceleration transducers from HBK were installed in the bogie and in the passenger compartment in the vertical and transverse directions.

The MGCplus data acquisition system was used for signal conditioning, together with HBK catman® software. This allowed the measurement results to be read off directly and prepared for further processing by programs such as MATLAB®.

The speed of the metro was logged by MGCplus and the time was recorded internally. A total of 3.5 million measured values were logged and managed, at a sampling rate of 400 measured values/s per channel. This means that at a maximum speed of 80 km/h, data is logged after only traveling about 55 mm.

Once the tests were completed, HBK‘s equipment proved that all the analyzed units satisfactorily met the UIC-518 railroad standard.

Company

A UNIVERSITY ATTUNED TO THE LOCAL AND GLOBAL AGENDA Founded in 1960 and the first university in Antioquia to obtain High Quality Accreditation from the National Education Ministry, Universidad EAFIT is an institution that is convinced that academic excellence, the strengthening of faculty teaching and research efforts, and an improved national and international presence are key pillars for impacting communities

Technology used

Other case studies