arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

SHP opts for QuantumX from HBK for bridge monitoring

SHP, Czech Republic

Introduction

Static and dynamic load tests completed in record time

chevron_left
chevron_right

It was an extremely short time window: Only five days were allowed for static and dynamic load tests on a new bridge across the Nitra river to be conducted by the Czech company SHP.

This meant: Two teams performed measurements and tests 24/7. SHP was able to provide its contractor with a detailed analysis already the very next day. One of the secrets behind the success: utilization of HBK's QuantumX data acquisition system for measurement. 

Motorways and expressways are the backbone of a country's economic success. For this reason, the Czech Republic has continually invested in the development of national primary routes since the political change in 1989. With success: The motorway and expressway network has since doubled to over 1,000 kilometers.

However, there's more to it than expansion: For quite some time, the Czech state as a contractor has paid attention to low, predictable costs and short construction periods in road construction - at the same time ensuring compliance with all relevant safety standards.

Therefore, significant static and dynamic load tests are a must prior to opening a bridge to traffic.

SHP as a partner for the safety of bridges

The Czech company SHP provides safety when it comes down to such tasks. The company, founded in 1991, is located in Brno and offers a wide range of services, for example, static load tests on bridges as well as long-term monitoring and other road construction services.

Since 2011, SHP relies on an own ultramodern laboratory for doing static load tests with highly skilled staff, analysis software developed in house - and HBK measurement technology.

An example is the bridge monitoring project at the R1 expressway from Nitra to Banska Bystrica in 2011. Here, the primary aim was to check the proper functioning and safety of 24 bridges modernized within the framework of the construction project.

The first three street sections' short construction period was a particular challenge. Here, SHP engineers were granted less than two months for checking the bridge structures' load-carrying capacity.

Static and dynamic load tests in only five days

This is an enormous challenge - especially since one of the bridges across the Nitra river is over 1 kilometer long.

SHP performed static load tests on this bridge within 4 ½ days and, in addition with an external partner, dynamic tests that needed to be completed within half a day.

To enable this short time window to be optimally utilized, two SHP teams took measurements on the bridge 24/7.

And, in addition: SHP was able to provide its contractor with a final analysis report directly the following morning after completion of the load tests.

The secret behind the success: HBK measurement technology

The test and measurement equipment used is a key success factor allowing for short response times. For this reason, SHP opted for HBK's ultra-flexible and compact QuantumX MX840Aamplifier for its static load tests during which displacement transducers, in particular, were installed at the bridge.

QuantumX combines all the characteristics that are required to manage ambitious measurement projects with short deadlines: Advanced Plug & Measure technology enables sensors to be quickly connected to the instrument - and automatically identified.

Measurements can be started quickly and analyzed just as swiftly. Furthermore, QuantumX - thanks to its compact size - is the ideal solution even for mobile applications at bridge structures or in other monitoring projects.

QuantumX, combined with catman®AP measurement software, also from HBK, allows fast data visualization, processing and subsequent use for final reports.

Company

SHP are an independent engineering consultancy specialized in designing of bridges and engineering structures and buildings. We design elevated roads and highways, railway viaducts, urban bridges and footbridges, from concrete and steel, as well as from timber. We design both small bridges and long viaducts, bridges over deep valleys, rivers and fjords.

We are specialised in arch, shell, cable-stayed and suspension bridges and roofs. Moreover, we have vast experience in designing high-rise buildings, roofing of stadiums, multifunctional buildings and other special civil structures.

The structures we have designed can be found not only in the Czech Republic and Slovakia, but also in the European Union countries, the United Kingdom, North and South America and Asia.

Strasky, Husty and Partners Ltd. (SHP)

Technology used

Other case studies