arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

HOERBIGER: Multi-component transducers for a transmission test rig

hoerbiger, Germany

Introduction

In industrial plants, usually only one load component is measured. Then extensive mechanical decoupling of the parasitic influences may be necessary.

chevron_left
chevron_right

2-component transducer for the synchronization process simulating test benches

Various transducer designs with different nominal (rated) measuring ranges and nominal measuring range conditions are used for the components. HBK has developed a 2-component transducer for the synchronization process simulating test benches made by HOERBIGER, the transmission manufacturer and the associated components.

This has been designed in such a way that axial force and friction moment are acquired simultaneously. The transducer also had to fit in the tight mounting clearance of existing test benches and needed the input shaft to run through a central hole. The oil mist environment and the presence of hot oil surrounding the lower half of the test benches were major challenges for which HBK found a good solution. The transducer achieves extremely good accuracy, with a composite error of ≤ 0.05 % f. s. and an equally low reversibility error.

Temperature sensitivity during operation, when the oil reaches temperatures of up to 110 °C, is also extremely low. Very good stability is certified during the entire service life test of several thousand cycles. The crosstalk, that generally limits the accuracy of multi-component transducers, has been minimized in all phases of development and manufacture. In order to further reduce measurement error during operation, an individual compensation matrix is needed for each multi-component transducer. This is included in the scope of supply, together with the sensitivity and the crosstalk as a percentage.

The output basis for the compensation matrix is the straight lines determined from the measured values, in accordance with the best-fit method.

About HOERBIGER

HOERBIGER's performance-critical products and services enable customers and partners from various industries to improve the performance and safety of their products and operations, save energy, and reduce emissions. This is how HOERBIGER enables change. For a better tomorrow.

More about HOERBIGER

Technology used