arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

QuantumX in the field test: How can the design of auger-drilling machines be improved?

kai le vehicle, China

Introduction

Kai Le Vehicle Co is implementing the use of HBK’s modular QuantumX data acquisition system to improve its technologies for investigating possible design improvements. The decision follows a series of demanding tests to hydraulically operated, cantilevered, heavy-duty, auger-drilling machines.

Kai Le Vehicle Co – which produces more than 6,000 units each year – decided that optimum results could be obtained from field tests with various loads applied to the cantilever arm of the auger-drilling machine. These requirements demanded equipment that was very robust and capable of accurate measurements in harsh ambient conditions.

chevron_left
chevron_right

The challenge

In addition power constraints meant that the supplied DAQ system needed to be battery operated with a continuous service life of at least four hours.

Additional equipment needed included strain gages and other sensors to record and capture voltage, current and temperature as well. These requirements meant that a minimum of 40 channels was needed along with post-processing software for further data analysis.

The HBK solution

To meet these demands HBK supplied four of its MX840A universal amplifiers. These highly ruggedized, 8-channel amplifiers are compact and give outstanding flexibility, measurement performance and ease of use making them ideal for this application.

In addition a QuantumX MX1601 was supplied as this provides 16 individually configurable channels for active sensors. The amplifier offers sample rates up to 19.2 kS per channel and a bandwidth of up to 3 kHz. Each channel is electrically isolated and every channel has a 24-bit Delta Sigma A/D converter.

Each of the different modules in the QuantumX series benefit from Advanced Plug and Measure along with automatic transducer and sensor identification via TEDS making system configuration easy. In addition all QuantumX modules benefit from a comprehensive software package including the free QuantumX Assistant.

To complement the QuantumX modules, HBK also supplied a CX27 gateway module to provide real-time data acquisition using EtherCAT for reliable results.

A locally sourced Lithium battery cell was provided for the mobile power supply as this exceeded the customer’s requirements.

The resulting configuration supports a maximum of 48 channels for data recording across a wide range of operational parameters. All channels are simultaneously acquired via internal bus with the measured data transferred via Ethernet protocol into a PC or laptop utilizing the CX27 gateway module.

The analysis of the results is carried out using HBK’s nCode GlyphWorks. This is a modular system enabling visualization and data manipulation along with frequency spectrum analysis and filtering capability.

Notes Zhang Yu Ming, HBK’s Business Development Manager for Test & Measurement in Shanghai, “We are really pleased to be able to support Kai Le Vehicle Co with this robust equipment that has proved reliable and very accurate in field tests”. He adds that HBK’s ability to supply a turnkey solution that utilized locally sourced components ensured that the customer was completely satisfied.

Technology used