arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Testing of a Suspension System Specifically Developed for an Electrically Driven race car

The Lessius Racing Team (LRT), Belgium

Introduction

The Lessius Racing Team (LRT), a group of enthusiastic students from Lessius Mechelen | Campus De Nayer, is taking part in the Formula Student Competition, an educational competition requiring students to build a race car prototype as a team, and then sell it. The mission of the Formula Student competition is to encourage young people to step into the technical business world, challenging them to design, build, finance, present, and compete as a team with a small, single-seat race car in a series of static and dynamic events. LRT is participating in the 1A class, meaning they will develop new and novel powertrain technologies that result in race cars with low carbon emissions, as defined by the Class 1A rules.

chevron_left
chevron_right

Validation of FE Models by Using Strain Gauges

A crucial part of designing an efficient race car is the suspension system. It plays a part in reducing both weight and friction, optimizing vehicle performance. To reduce not only the total weight of the race car, but also the so-called unsprung mass, as little material as possible has to be used in the construction of the suspension system. A low unsprung mass is important, to ensure fast response of the suspension system to bumps and potholes, maintaining constant contact of the tires with the racetrack, and providing maximum vehicle control. The stiffness of the suspension is another important part, as deformation in the suspension would influence the geometry of the car setup (such as caster, camber, and toe), which would adversely affect handling and rolling friction. In addition, the suspension has to handle all the forces acting on the race car to keep it on track when turning into corners at high speed. To ensure the maximum weight reduction does not affect the structural strength, modern finite element (FE) simulation packages have been used in the design. Only one link in the chain for developing a sturdy, but lightweight, suspension was missing: validation of the FE models to ensure the models and the design are correct. This validation, offering certainty about the design that the team was looking for, has been achieved by applying strain gages to different suspension parts. The choice was made to perform a test with direct loading by putting weight on the vehicle while measuring the force actually acting on the full suspension with weighing plates under the wheels.

Further Tests for Increasing the Vehicle Performance

The measured forces acting on the wheels were used as input parameters for the FE model simulation to correlate the material deformation measured by the strain gauges with the corresponding locations in the FE model. This approach offers a well-defined test scenario that simplifies the correlation of simulated and measured data. The next step is to instrument the race car with further data-acquisition equipment to perform measurements in real-life use cases  actually driving the vehicle on a race track. This has already been discussed, and will be an assignment for next year's racing team. For now, the static tests have proven to be a great success, and ensured structural stability of the current suspension design. Further dynamic tests will help the team minimize the weight and increase the vehicle performance without risking component failure or vehicle misbehavior due to a lack of structural stiffness.

The Lessius Racing Team (LRT)

 

Technology used