arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

SISU AXLES: heavy-duty planetary axles

SISU AXLES, Finland

Introduction

Sisu Axles had previously used a test bench that simulated and measured how various loads strained the axles. However, the torque data this test bench produced was not reliable or accurate enough for the team’s needs because it had to be collected from the control system by measuring the electrical output to the inverters.

chevron_left
chevron_right

Vehicle Axles Must Withstand High Forces and Have More Torque Capacity

Sisu Axles manufactures heavy-duty planetary axles for vehicle types ranging from trucks and container handling equipment to military vehicles.

Such axles are subject to tremendous forces while carrying heavy loads. Increasing competition among vehicle manufacturers has forced them to make their vehicles more economical and efficient.

Therefore, the modern axles that go into these vehicles must be more durable and offer greater torque capacity.

To ensure their new axles meet the increasing demands of their customers, the product development team at Sisu Axles needs accurate measurement data.

The HBM T40 Torque Transducers

Sisu Axles rebuilt their test bench by installing the T40 torque transducers from HBK to produce more accurate measurements more easily.

The test bench, which allows testing one axle or one axle component at a time, consists of a 193 kW electric drive motor plus two 98 kW electric motors, which act as brakes, replacing wheels.

The drive motor represents the vehicle’s engine; the braking machines simulate the stresses caused by the loads from tires.

The product development team can change test setup as needed, such as by using the braking machines as drive motors and adding any gears needed to generate a suitable ratio.

 

Reliable Measurement Results

The T40 torque transducers measure torque from the flanges of the electric motors. The MP60 amplifiers from HBK condition all torque signals from the sensors, which are transferred to the system via an analog output.

The T40 is the optimal device for torque measurements in a test bench because It provides reliable measurement results, even in the most extreme conditions, such as those caused by surrounding electric disturbances, vibration and temperature.

The small size of the T40 makes it easy to integrate into test benches. The sensors also have good resistance for axial and radial loads. The T40 requires no maintenance because its structure includes no wear parts.

The Accuracy Product Development Demands

"It is essential for the product development that design data can be verified in a test bench. We can make sure that what has been calculated takes place in practice. With the data we receive, we can save in production costs. Accurate and real-time torque data is extremely important to us,” says Jouni Teppo, director of R&D for Sisu Axles Inc.

According to Teppo, the biggest advantage of the HBK T40 torque transducers is that they offer a sufficiently high level of torque and accurate measurement data.

With their old test bench, the measuring error could have been several percent; today, they can achieve 0.05 percent accuracy.

 

Wireless Data Transmission

According to Teppo, one of the benefits of the T40 torque transducers is that torque data can be transmitted wirelessly from the test bench.

The digital torque data signal is transferred wirelessly by telemetry from rotor to stator. The compact size of the T40 allows it takes up little space in the test bench. Together, the size of the T40 and wireless data transmission capability simplify both transducer installation and test bench operations.

Sisu Axles’ new system is also easier to integrate with existing measurement systems and electronics by Fieldbus.

 

Continuous Availability

"In addition to accurate data and wireless transmission the third important benefit of measurement solution from HBk is, that it is available all the time.

Real-time measurement data is displayed on the PC screen and it can also be stored into the measurement database,” Teppo concludes.

Advantages with HBK

  • Reliable results even in the most extreme conditions
  • Easy to integrate into test benches and completely maintenance-free
  • Accurate and easy measurements

Company

Sisu Axles are a world-wide player, with applications using their axles on every continent from the United States to Australia. they provide high quality, short lead time, flexibility and excellent product performance based on strong application know-how used in engineering.

Sisu Axles is an independent axle manufacturer for heavy duty truck, military, container handling and industrial applications. They specialize in heavy duty planetary reduction and independent suspension axles.

Jouni Teppo Director of R&D for Sisu Axles Inc.

Technology used

Other case studies