arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

High Octane- Torque Measurement of Drive Shafts

High Octana Motorsports, germany

Introduction

High-Octane Motorsports e.V. is the Formula Student team of the Friedrich-Alexander University Erlangen-Nuremberg (FAU). Formula Student is an international engineering design competition in which teams of students from different universities compete against each other in static and dynamic disciplines with the formula racing cars they designed and built.

Sensor data plays a central role in developing and driving a competitive racing car. For this reason, strain gauges are installed at the latest vehicle’s drive shaft to enable the torque of the internal combustion engine to be measured. Up to now, exact engine performance data could only be determined on the test bench but not during tests on the track. To achieve this, a lightweight and compact solution was required that could be integrated as easily as possible into the racing car and the electronic system.

chevron_left
chevron_right

Measurement setup

Strain gauges of type XY2/XY4 proved to be the right choice to meet these requirements since they enabled measuring the drive-shaft torsion for extrapolation of the torque applied to the drive shafts and the corresponding engine torque. The strain gauges were wired in a bridge circuit and connected to a battery-operated telemetry transmitter. The measured values could be recorded and stored using the vehicle's on-board telemetry receiver. The sensors were provided by HBK, and the telemetry equipment was provided by another manufacturer.

Installation

The DAK1starter kit from HBK was used to make strain gauge installation as easy as possible. The kit contained everything except the strain gauge that was required for measuring torsion in this application. Therefore, preparing the measuring points on the drive shaft and subsequently installing the strain gauges were very easy. After checking the strain gauges and connecting them to the telemetry transmitter, the measurement setup was covered to protect it from moisture and mechanical influences during its use in the harsh proving-ground environment. In this application, centrifugal forces on the rapidly rotating drive shaft also played a major role. The cables were strain-relieved using the X60 superglue included in the kit and fixed with textile tape using the AK22 covering agent. The setup was then calibrated for torsion and installed in the racing car.

Testing

Initial data could be collected in tests with the racing car on the track. They provided information on both the behaviour over time and the amount of torque applied to the drive shafts. The data log showed, for instance, the torque to a drive shaft, the speed, the engine speed, and the accelerator pedal position over time. This enabled the engine torque to be determined at any time during operation in the racing car. On the one hand, the power values of the engine on the test bench could be compared directly with those in the vehicle, thus enabling the transmission losses in the racing car to be calculated. On the other hand, this allowed changes in engine torque during the tests to be objectively detected. This enabled the quantification of the impact of changes in the internal combustion engine's application on the engine torque at certain rotational speeds and perfectly complemented the driver's feedback by ascertaining their assessment by numerical values.

Unexpected variations in engine performance could also be detected at an early stage and responded to accordingly. For instance, an incorrect chain tension could be detected. Furthermore, the drive shaft design could also be validated by torsion measurements; in particular, the stress peaks occurring in the drive train could be quantified. The collected data allowed for further optimization and, thus, reductions in weight. The collected data could also help adjust the differential gear. During cornering, the maximum transferable torque differed between the two powered rear wheels. The difference in torsion between the left and right drive shafts allowed the drive torque transferred to the respective wheel to be extrapolated and, thus, the optimum degree of locking of the differential to be determined and adjusted. The data obtained also helped optimize the self-developed lap-time simulation. This significantly supported design decisions and consequently the development of the racing car. The three performance values determined in the test run could be used to validate and further optimize the simulation model and to obtain even more precise simulation results.

The impact of various dynamic parameters on the achievable lap time could be calculated with as precise a simulation as possible. This information enabled future racing cars to be made even faster. The test runs for measuring the torsion using strain gauges on the racing car’s drive shafts during the previous season enabled the team to gain valuable insights which have proved to be very helpful in installing the strain gauges in the racing car under development. Along with the application in the drive train, there were also other areas, such as in the chassis, where stress and strain measurements allowed for optimization in terms of lightweight construction and stiffness. Due to the support of HBK who provided the required components, the young engineers of High-Octane Motorsports e.V. were able to gain valuable experience and insight into HBK’s product portfolio and the potential applications.

High Octana Motorsports

High-Octane Motorsports e.V. is a registered, nonprofit organisation and also a university group at Friedrich-Alexander-Universität Erlangen-Nürnberg.

As a Formula Student team, we have been building an innovative race car every year since our foundation in 2007. All tasks necessary to achieve this goal are solved within the club and without any professional help. Our members develop their own concept, design in CAD and manufacture the race car. The car undergoes various tests before the races to ensure safety and performance. The club is composed of students from all faculties of the university, who work independently to acquire specialized knowledge and learn practically about automotive engineering, manufacturing technologies and economics. This interdisciplinary combination of the technical and economic fields is unique and a characteristic of Formula Student, in which the race car is evaluated not only from a technical point of view, but also from a financial one.

More about High Octana Motorsports

Technology used