arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Green shipping: Saving fuel with precise torque measurements

The marine industry is in a state of transformation around the world. Mandatory step-by-step reduction of pollutant emissions produced by shipping traffic has been regulated by the international MARPOL Convention. This has led to an advance in engines that are able to burn different types of fuel such as Liquefied Natural Gas (LNG). The gas supply to the engine can be controlled using a precise load signal from the drive shaft. This makes it possible to achieve the required reduction in pollutant emissions. HBM has developed a torque transducer specially designed for to adhere to these regulations in the marine industry, theT40MAR. Within a few years, emission levels in shipping will have to be drastically reduced, according to the requirements of the MARPOL Convention. To comply with these requirements, the marine industry is following two different approaches:
  • After-treatment of exhaust gases for conventional drives
  • Development of new, cleaner drives

Alternative drives on the rise

After-treatment of exhaust gases for conventional drives refers to exhaust gas recirculation, particle filters and catalytic converters. Expensive components must also be installed for this purpose. The challenge is to achieve the lowest possible fuel consumption to operate them. The development of new, clean drives is led by engines that are able to burn different types of fuel, such as all conventional marine fuels plus LNG. The advantage of this type of drive is that it burns very cleanly, making it possible to achieve the required lower exhaust gas levels easily. LNG is also more costeffective than oil and will be available for longer in the future as a resource. Engines that can burn different types of fuel must be able to switch quickly from one fuel to anotherwithout any loss of power. When the engine is running in LNG mode, critical operating states must also be reliably prevented. This is achieved by a sensitive controller whose most important element is a load signal with very low tolerances. This ensures that depending on the navigating situation, the engine is always in an optimum operating state. Additionally, this offers considerable fuel savings.

Load signal generated by torque measurement

The rotational speed and torque must be measured to generate the load signal. Until now the torque of large marine engines has been determined indirectly, by measuring auxiliary quantities and then calculating torque. The disadvantage of this is that the measurement uncertainty is very high and very difficult to verify. Installing a measurement flange calibrated to the torque as a measurement directly onto the drive train enables direct and very precise measurements with measurement uncertainty that can be clearly demonstrated. An overall measurement uncertainty of well under 1 % can be achieved, as the accuracy class of the torque transducer itself is 0.1. The very short signal run times also make it possible to implement control commands quickly. HBM offers a torque sensor for use with the T40MAR, specially developed for the drive systems of ships. The transducer has analog and digital signal outputs and allows for direct torque measurements up to 400 kNm. T40MAR is easy to install and parameterize. Measurement signals are also transferred without contact.

Certified for use in shipping: the T40MAR torque flange:

Related Products

No more result to load