arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Aqira - Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Torque measurement in ship lifts

Shuikou dam, China

Introduction

Reliable, stable and robust: HBKtorque sensors have worked well in Shuikou dam ship lifts for more than 10 years.

chevron_left
chevron_right

In many power machinery and transport machinery such as motors, fans, pumps, gearboxes, automotive drive shafts, marine propeller shafts and oil rigs, the torque in drive shafts is an extremely important parameter for the entire power system. A boat lift, ship lift, or lift lock is a machine for transporting boats between water at two different elevations, and is an alternative to the canal lock and the canal inclined plane. A vertical ship lift is large electromechanical equipment for a cargo ship passing dam. It's composed of four parts which includes an upper lock head, lower lock head, ship reception chamber and the main lift system. The main lift system consists of lifting equipment, corresponding control equipment and testing equipment distributed in four lifting points. Each lifting device at different lifting point includes DC motor, reduction gearbox, hoist drum wrapped lifting rope and hydraulic brakes.

In order to operate a ship reception chamber synchronously (including electrical synchronization), smoothly and safely, the output shafts of reduction gearboxes at four lifting points should be connected to a closed rectangular shaft system which constitutes mechanical rigid synchronous system.

To ensure power equilibrium, make sure torque outputs of drive motors for the mechanical synchronous drive system remain the same. It is important that the synchronous transmission shaft does not suffer excessive torque and rupture.

When a winch motor fails, the other three winch motors will supplement power to the failed lifting point via synchronizing shaft system immediately in order to ensure normal operation of the main hoist. Synchronizing torque shafts is monitored and reflects the power allocation.

In order for the ship to avoid sinking or floating when the brake releases, the drive system will generate a certain torque output in advance according to unbalanced force and its direction between the ship reception chamber and the balancing weight.

The HBK torque transducer T40FM was used in the Silin dam ship lift (Capacity: 500tons, Dimensions of navigable ship: 55×10.8×1.6metres, vertical lift: 76.6metres) in China. Four HBK T40FM torque transducers were installed into rectangular ring synchronized shaft systems to monitor the working torque of each synchronized shaft. The torque signals are used for monitoring applied torque, controlling equilibrium torque and triggering an alarm if the limit torque is exceeded.

Benefits from HBK’s T40FM

  • Reliable and stable: HBK torque sensors have worked well in Shuikou dam ship lifts for more than 10 years.
  • High precision: accuracy class 0.1 with linearity 0.1%, reproducibility 0.05%, Tcspan 0.1%/10K, TC0 0.05%/10K ensures the best torque measurement result
  • High frequency response helps fast control
  • Robust: excellent ability for overload and parasitic load
  • Easy installation

 

Benefits from HBK’s service team

  • Free maintenance
  • Quick response
  • Professional consultation,
  • On-site support

The Shuikou Dam is a concrete gravity dam on the Minjiang River in Fujian Province, China. The primary purpose of the dam is hydroelectric power generation and it supports a 1,400 MW power station with 7 x 200 MW Kaplan turbines. The dam also provides navigation with a 500-ton flight of 3 ship locks and a 500-ton ship lift. Other purposes include flood control, irrigation and recreation.

Technology used

Other case studies