arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Innovative: Viticulture robot for the cultivation of steep slopes

geisenheim university, germany

Introduction

HBM Sensors and Software Enable Tenth-of-a-Percent Precision in Geisi Robot

chevron_left
chevron_right

Geisenheim University has developed a new concept for mechanized work on steep slopes: the viticulture robot "Geisi". Geisi shall have the capability to work on slopes of up to 70 percent - remote controlled and without ropes.

Viticulture on steep slopes has shaped the landscape in Germany's wine growing regions. However, the proportion of cultivated steep slopes is steadily decreasing. In 2010, it was down to only 9 percent of the overall area under cultivation. One of the reasons for this is that working these steep slopes is completely done by hand - work that is dangerous, physically demanding and costly. The Institute for Technology at Geisenheim University, however, intends to remedy this situation by substantially facilitating the landscape-shaping viticulture on steep slopes. A team headed by Professor Schwarz set out to develop a new concept for mechanized work on steep slopes: Geisi. Unlike earlier equipment for mechanized cultivation, Geisi is designed to work remotely and without ropes on slopes with grades up to 70 percent. This leads to significant savings in labor cost and at the same a valuable plus in work safety. A fleet of never-tiring, mechanized steep-slope viticulture robots can offer long-term advantages as well with their ability to autonomously perform typical tasks such as crop protection, mulching or foliage work. Geisi is designedto be available at a substantially lower price than earlier mechanized systems built to work on steep slopes. To make these goals a reality, the project managers got HBM on board. Strain gauges and the rugged, mobile Somat eDAQ data acquisition system from the test and measurement expert make an important contribution to enabling Geisi to autonomously and reliably move on steep slopes.

null
null

Unique concept for mechanized viticulture

Spiked rollers, commonly used in alpine slope mowers, form the basis for the multifunctional transport and drive system that supports persons working on steep slopes. The rollers have an integrated drive train. This guarantees an extremely low center of gravity of the vehicle, which, besides the excellent interlocking of the spiked rollers with the underground, is an important prerequisite to Geisi's rope-less operation on extremely steep slopes. Pairs of rollers each arranged one behind the other allow the innovative tool to safely and optimally move on slopes. For this purpose, the development team first had to modify the drives of the spiked rollers to enable the two- or three-axle Geisi to maneuver as desired.

null

Test and measurement technology from HBM is pivotal

The steering system of the all-wheel driven work platform on spiked wheels posed a special challenge to the Geisi development team. A skid steer system with rollers running at different rotational speeds on the left and right hand side proved unsuitable because of the spiked rollers' strong interlocking with the underground. The prototypes were fitted with comprehensive test and measurement equipment for documentation and analysis of the material loading during use. Strain gauges from HBM were installed on the axles used as drive roller suspensions to allow three-dimensional acquisition of the occurring forces and moments. Additional data that was recorded included geographic coordinates (via GPS) as well as CANbus communication and inclination. The rugged, mobile Somat eDAQ amplifier system from HBM was used for data acquisition. The collected information enabled both speed and slip to be computed and resulting in improved programming for precise steering including safe negotiating of curves. The forces resulting from maneuvering during the test runs were too great, material loading was too high. A passive, articulated steering system without hydraulic cylinders with two crossover stationary and two moving rollers proved to be the ideal solution. It provides a high degree of mobility and reliably prevents slipping of the rollers not used for steering.

nullnull

More images

nullnullnull

Recommended for you

No more result to load