arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

HBM Enables Jungheinrich to Take Product Quality to the Next Level

jungheinrich, germany

Introduction

Jungheinrich is a world leader in fork lift truck, warehouse, and material flow technology. The listed company provides innovative warehouse logistics solutions offering high functionality, reliability, and excellent quality. These are the result of extensive testing prior to and also after the market launch of new products. Jungheinrich, for instance, relies on extensive product testing at the customers’ premises. The insights about actual loads in day-to-day operation gained under real conditions are not only used to validate the values forecast during product development, the specialists also use the practical test results to continuously improve their products. For measurement and analysis, Jungheinrich relies on high-performance solutions from HBM such as the universal QuantumX data acquisition system.

chevron_left
chevron_right

EJE Series Collects Practical Data in “Undercover Operation”

The innovative EJE series of high-performance electric pedestrian pallet trucks from Jungheinrich allows customers throughout the world to load and unload trucks and to transport pallets over short distances. The pallet trucks feature a maintenance free three-phase AC motor and particularly efficient, easy and, safe handling in confined spaces. Furthermore, the innovative EJE 116 to 120 pedestrian trucks, regardless of their compact dimensions, offer a striking capacity of up to 2 tonnes. The EJE series’ outstanding performance data is, amongst other things, a result of the fork lift trucks’ excellent quality and continuous optimization. This is why the company performs extensive series of tests, not only during development. As part of their quality assurance and further development program, Jungheinrich collect valuable data directly on site at select customers - upon consultation with the customer and in compliance with applicable data protection guidelines. Jungheinrich acquires the required data on the actual device structure in practical use and virtually “undercover” - without any effort to the user or loss of performance. The measurement electronics, invisibly integrated in the pallet truck, autonomously takes the required measurements in day-to-day use.

Clever product testing solution

When it comes to load data acquisition, Jungheinrich relies on HBM. The QuantumX CX22B-W stand-alone data recorder plays a key role in this. 

null
nullnullnullnull

HBM on Board with Jungheinrich Quality Assurance Program

Jungheinrich relies on HBM in determining the load data of all vehicles and type series in practical use. The QuantumX CX22B-W stand-alone data recorder is the heart of the test and measuring equipment used in this “undercover operation”. The compact measurement modules are  distributed and invisibly integrated behind the pallet truck cover. The data recorder stores the test data that is either supplied by strain gauges, pressure transducers, current, voltage, acceleration, and temperature sensors or taken from the CAN bus directly in the device. Neither connection to a PC nor user intervention is required - the system operates fully autonomously in the background. After about two weeks regular day-to-day use, the real-life data is read out on site at the customer’s premises. The goal for the future is to implement this via remote access (cellular network) to further reduce personnel requirements. The data packages are subsequently analyzed using nCode GlyphWorks software from HBM, a powerful tool for test data analysis in engineering with a focus on durability and fatigue life analysis. The analysis results allow valuable conclusions to be drawn about how loads affect the structure of a product in practical use. Both the values forecast within the scope of simulations in the development stage and the values determined in the test bench can thus be validated on the basis of actual data acquired in practical use. In addition, the insights gained under real-life conditions provide a basis for the further improvement of products from Jungheinrich.

Everything from a single source

Jungheinrich has been using reliable test and measurement equipment from HBM for several years now. On the one hand, this is due to straightforward collaboration and fast response to inquiries. On the other hand, HBM provides everything from a single source, complete solutions for the entire measurement chain as well as components offering universal use, scaling, and convenient configuration. Moreover, HBM test and measuring equipment is outstanding for its reliability and high performance. One example of this is the QuantumX data acquisition system used in field testing of EJE type series electric pedestrian pallet trucks: It provides compatibility with the Jungheinrich CANopen bus and, in addition, fast disassembly, high sample rates and up to 512 GB memory capacity. Wireless routers can easily be connected via Ethernet at any time.

Jungheinrich is a world leader in fork lift truck, warehouse, and material flow technology. The listed company provides innovative warehouse logistics solutions offering high functionality, reliability, and excellent quality. These are the result of extensive testing prior to and also after the market launch of new products.

For more information visit: https://www.jungheinrich.de/

No more result to load