arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Aqira - Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All Aqira See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Jaw Crusher in Road Test: Reliable Measurement Results Under Challenging Conditions

Terex®MPS, usa

Introduction

The Largest Tracked Mobile Machine

The rugged data acquisition system SomatXR guarantees reliable measurement results in harsh environments during long term tests of the jaw crusher LJ5139 from Terex®MPS.

When Terex® MPS needed a reliable and flexible system to measure stress on its range of stone crushing machines, it turned to HBM to provide a solution. As part of its ongoing research towards the development of this powerful range, HBM was asked to consult on the LJ5139, which will be the largest tracked mobile machine in its range when fully developed. 

chevron_left
chevron_right

The Challenge: Uneven Surfaces, High Impact Forces, and Dust

The issues being faced by the LJ5139 Jaw Crusher which was used in a quarry, were varying in nature. With the machine itself weighing up to 110 tonnes, the chassis is subject to high loads when tracking on uneven surfaces. In addition, the hopper and feeder receives high impact forces when large stones, with a volume of up to 1 cubic m are dropped from the excavator which is used to feed it. Moreover, the crusher itself is subject to forces of up to 8000 kN during the crushing process.

“To deal with these issues, we initially made use of Finite Element Analysis during the design process and verified the results in the field using strain gauges. Previously relying on rented equipment, we were keen to invest in our own equipment for increased flexibility.” said Ian Boast from Terex Corporation.

Furthermore, the initial equipment being hired was susceptible to noise interference from surrounding equipment. This was particularly problematic as the loadings in the crusher are often random and transient in nature which could potentially cause confusion and false results. In addition to this, the physical environment in the quarry,  which is arduous with high levels of dust, not only limits the test options on site, but also requires extra care to be undertaken with the conventional equipment being used. 

Reliable Despite Sudden Knocks and Power Failure: SomatXR

After a study of the issues faced, HBK specified its DAQ, SomatXR series, which is particularly suitable for use in harsh environments. To complement this package, HBK also suggested the SomatXR MX1615B-R module and related accessories, which included RF-9 strain gauge rosettes. Given the demanding environment, it was important to choose the correct equipment available. Often faced with wet and arduous conditions, the ability to operate reliably, despite sudden knocks, was a key consideration. When operating under such extreme conditions, it is also often hard to anticipate all of the problems that may occur, such as losing measurement data due to unforeseen events, such as a power failure.  This is a particularly relevant feature in terms of long term tests, such as those required by Terex® MPS. The SomatXR system enables data to be continuously recorded.  This means that should a failure interrupt a test, recorded data up until that point will be saved. This is particularly beneficial as it also means the system should also continue data logging automatically, after the interruption, without any need for user interaction. HBK data acquisition systems are suitable for a wide range of mobile testing applications but the immense load requirements and extreme environmental conditions surrounding Terex® MPS did present a challenge. However, thanks to HBKs extensive experience in mobile testing and demanding fields, it was able to provide a solution which offers Terex® MPS the flexibility of being able to work around available and convenient testing windows. In addition to specifying and supplying Terex® MPS with a system to meet its needs, HBK also provided engineers with training and support.

Terex®MPS

In April of 2009, the Cedarapids, Simplicity and Canica brands were brought together under the Terex MPS umbrella to carry on their rich tradition of offering comprehensive solutions. Together we provide a complete range of crushing and screening equipment to customers around the world operating in four key industries: mining, aggregates, demolition and recycling and industrial minerals. Our equipment is designed to produce the highest quality end products in processing hard and soft rock, sand and gravel, ore and industrial minerals. 

We provide Modular, Portable and Static equipment – plus full parts, service and maintenance with support you can count on, wherever you are. 

More about Terex®MPS

Lan Boast

Technology used