arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management
null

Mobile Data Acquisition Using Strain Gauges and the QuantumX From HBM

TU Darmstadt racing team e.v., germany

Introduction

The TU Darmstadt Racing Team (DART) is a group of university students from the Technical University of Darmstadt that have been participating in the Formula Student international design competition since 2005. Students from various disciplines have been independently working on developing and producing an electrically powered Formula racing car and have been competing against other teams from all over the world year after year.

chevron_left
chevron_right

Driven by the passion for motorsport, a new racing car will also be developed in the 2020 season. In September of 2019, DART, with the support of HBM, launched a project to validate and analyze the chassis using HBM equipment. To detect the forces acting in the wishbones and tie rods during driving, strain gauges (SG) were installed and the test vehicle was equipped with appropriate electronics. Future developments and the optimization of the chassis will be based on the collected data.

null
null

Strain Gauges

Type XY7 strain gauges were used for the tests and connected in a Poisson half-bridge to allow the absorption of tensile and compressive forces while ensuring temperature compensation. These types of wishbones and tie rods are designed exclusively for the absorption of tensile and compressive forces. After their installation, the strain gauges were wired with special measuring leads and calibrated by a Darmstadt-based institute. The strain gauges were protected using the SG250 covering agent by HBM and a cable from HBM (order no.: 4-3301.0151) was selected as the measuring cable. Furthermore, the strain gauges were provided with strain relief and protected with masking tape.

null
null
null
null

Measurement Electronics

The MX1615B Quantum X module and the CX22 data recorder were used to acquire and record the data. The modules were fixed in the vehicle and synchronized with each other via Firewire. A total of 13 channels were used in parallel.

null
null

After the setup and commissioning of all the hardware and software, test runs were carried out on an airfield where different test tracks were set up. To test as closely as possible to the conditions given by Formula Student and to identify the maximum loads, chicanes with fast load changes as well as wide curves were driven.

For example, the maximum forces recorded during the test in the right-hand tie rod were equivalent to 1702 N for tensile force and 961 N for compressive force. Comparing the data obtained by the measurements to those provided by the camera allowed the evaluation of which load case these values corresponded to. The maximum tensile force was measured during oversteering in a fast left-hander and the maximum compressive force in a wide right-hander at high speed.

null
null
null

The forces were also recorded when steering while stationary, with a maximum force of 1300 N being measured.

Due to the support of HBM, DART was able to collect further measurement data which are considered as the basis for further development. In the coming season, these results will be used, for example, to optimize all the wishbones and tie rods and design a steering actor for autonomous driving for the Formula Student Driverless competition.





Prospects

More tests using HBM equipment are planned for the future. For example further optimization iterations on the wishbones and tie rods, the development of completely new concepts with wishbones made of composite materials, and the strain or deformation analysis of other chassis parts are conceivable.

Exciting challenges are waiting for you!

HBM offers numerous opportunities for students, including internships or student trainee activities. Find out more about the various tasks and job offers.

Go to our career pages to find helpful tips for your application.

Recommended for You