arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

“E-Jet" Concept Vehicle by RWTH Aachen Fitted With HBK Sensors

RWTH Aachen University, Germany

Introduction

The "E-Jet” concept vehicle sponsored by Hans Hermann Voss-Stiftung innovates steering by providing an innovative actuator for a steer-by-wire system. Without a physical connection to the wheels in place, no mechanical feedback of the forces and moments associated with the tire-road contact can be gained.

This feedback helps the driver stabilize the vehicle. In order to ensure the driver's interaction with the vehicle, the steering bow was developed as an active actuator, which means that the steering bow movement can be influenced by an electromechanical actuator, which enables the steering bow to provide feedback on the vehicle’s driving dynamics.

chevron_left
chevron_right

The "E-Jet" project developed an ultra-light vehicle with a serial bio-hybrid drive in the form of a combination of electric and pedal drive. The steering lever, also known as the steering bow, specially designed for this project, offers a new driving experience. A reliable measuring system had to be developed to ensure precise input of the driver's force and thus the exact transmission of the steering movement to the vehicle.

With the MCS10-005-6C, HBK has introduced a multi-component transducer that enables both the measurement and analysis as well as the compensation and reduction of the given deviation forces.

The project resulted in the development of the steering bow. The multi-component sensor enables the precise transmission of steering movements. In combination with the calculation of the setpoints for the steering angle, the "E-Jet" becomes steerable and drivable.

Rheinisch-Westfälische Technische Hochschule Aachen (RWTH Aachen University) is the largest technical university in Germany with more than 45,000 students. With the ika, the" Institute for Motor Vehicles", the university has at its disposal an innovative testing facility for motor vehicles.

The institute is running research, among other things, on "Vehicle Intelligence & Automated Driving", "Vehicle Concepts & HMI", and "Energy Management & Drives".

In addition to the training of future car manufacturers, the ika aims to innovate the modern transport system, for instance, with the  „E-Jet" project.

chevron_left
chevron_right

Use of HBK’s Multi-Component Transducers in the Steering Bow

Only the tangential component of the actuating force is relevant for actuating the steering bow. Nevertheless, the use of a multi-axial force sensor is required in the current phase of development in order to detect, analyze, and compensate for the influence of deviation forces and moments.

In addition, it is essential that the measuring system is not only reliable but also capable of accurately recording the user’s force input. With an accuracy class of 0.2 and a compensation matrix for reducing crosstalk effects, HBK's 6-axial MCS10-005-6C multi-component transducer fulfills these requirements.

The Importance of Precise Measuring Instruments in the Steering Lever

The steering bow is designed as an active actuator with force input and displacement feedback. The driver receives feedback concerning the vehicle’s driving dynamics via the position change detected by the steering bow. This results in the subdivision of the steer-by-wire system’s control concept into two phases: setpoint setting and feedback synthesis.

 

Setpoint Setting

The force exerted by the driver on the handle element is measured using the multi-axial force sensor. Strain gauges allow for the measurement of forces and moments in the force sensor. These are then amplified, digitized, and evaluated in the real-time computer. Based on the sum of the forces on the left- and right-hand sides (with the sign of the force on the right-hand side being inverted since both sensors give a positive signal for the same direction of actuation), setpoints for the steering angles of the front wheels are calculated as a function of the vehicle speed and the vehicle geometry. In the "E-Jet" concept vehicle, these steering angle setpoints are implemented by steering motors.

 

Feedback Synthesis

The steering motors output the actually implemented steering angle that depends on the driving situation and the road conditions. Based on the actual steering angles of the wheels and the driving conditions the real-time computer calculates a setpoint for the steering-bow angle. This is implemented by the actuator at the steering bow.

Technology used

Other case studies