arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Material Testing with ZwickRoell

Zwick Roell is a global leader in material properties testing. The integration of HBK’s QuantumX data acquisition system raises the insights gained from these tests to a new level.

Static material testing machines are specially designed for tensile, compression and flexure tests, as well as for shear and torsional tests, so they are ideal for performing complex tasks in the field of material and component testing. But there are also dynamic and fatigue testing systems for specific application areas. Modular robotic testing systems are becoming increasingly common, allowing for the performance of efficient and reproducible tests. Customized solutions can be put together using standardized components.

System Topology of a Compression Testing Machine With Integrated QuantumX Module

Any QuantumX module can be integrated into a ZwickRoell tensile/compression testing machine. In the following example, the QuantumX MX1615B strain gauge amplifier is used to determine the strains of a material or coupon under load.

HBM strain gauges are attached on to the sample and connected to the bridge amplifier. In addition, other transducers or active sensors, such as RTD-resistant, temperature measurement transducers such as Pt100/Pt500/Pt1000, can be connected to gain further insights. The fully time-synchronized measurement data directly streams into ZwickRoell’s testXpert® III software.

Incidentally, the integration of the QuantumX family enables the test setup not only to acquire strain, but also force, torque, displacement, temperature, flow, pressure and many more physical quantities.

null
white check mark in green circle

Main Advantages of Integrating QuantumX into ZwickRoell Testing Machines

  • High flexibility, by simply adding any transducer/sensor

  • Highest precision due to HBK's patented technology

  • Complete measurement chain from one supplier

  • Versatile use protects your investment for many different setups

The enabled use of strain gauges and the flexibility of integrating any sensor in material testing, allows a new level of simplified measurement and testing.

The extensometers installed in the testing machine for displacement measurement mainly covers standardized samples. However, integrating the QuantumX MX1615B module opens the door to best-in-class strain measurement, taking advantage of patented wiring schemes as well as noise-suppressing carrier-frequency excitation technology.

The whole measurement setup can easily be scaled up by adding other or additional QuantumX modules.


Integration Workflow in catman and testXpert® III

The sensors of the QuantumX module are now listed under 'Machine'. If the channels were also created under 'Test specification', they are linked to the corresponding sensor and are ready for use.

To ensure that the strain gauge measures synchronously with the other sensors, a 5V signal is sent to an input channel of the QuantumX module and the returning signal is read in.

In testXpert®, all channels that are set to the default sample rate will later be visible. The maximum sample rate in conjunction with testXpert® is 1200 Hz.

To test the configuration, we suggest a test measurement and visualization.

To use the created measurement configuration of the QuantumX module in testXpert® III, it must be saved as a .mep file.

Read here what ZwickRoell says about the integration of additional measurement technology.

Recommended for You

No more result to load