arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Encounter with a rogue wave: HBK measurement technology ensures reliable results

Company name, Country

Introduction

chevron_left
chevron_right

Researchers of Hamburg-Harburg Technical University have simulated, in a spectacular test, the impact of a rogue wave hitting a cruise liner's window. HBK's Genesis HighSpeed system ensured reliable data acquisition during the test. Transparent, light weight, bright and spacious, large-size windows are increasingly being installed on large cruise liners which adds architectural value to the cruise line, however, raises many questions regarding the ship's design.

Wave impact is a particularly critical issue: What are the requirements for the design of ship's windows to be met to enable them to withstand the impact of large masses of water? Would the windows presently installed be able to withstand a so-called "rogue wave"? An encounter with a rogue wave - though extremely rare - is a conceivable scenario.

Ship accidents and encounters with occasional large "rogue waves" have time and again been reported over the past decades: reality or sailor's yarn? Only since September 11, 1995, when a rogue wave hit cruise liner Queen Elizabeth 2, is this phenomenon considered scientifically validated and proven. Research of the topic has just begun - covering various aspects of ship design as well. What are the design requirements for ship components, for example, windows, to enable them to withstand the enormous force of a rogue wave hitting the ship? Can a window withstand a rogue wave at all?

There is an increasing need to answer these questions, now more than ever since large are increasingly being installed on modern ships. A research project led by Professor Wolfgang Fricke of the Institute for Ship Structural Design and Analysis of Hamburg-Harburg Technical University investigates the questions arising from the use of increasingly large windows on ships - also considering wave impact and even an encounter with a giant rogue wave.

Spectacular drop test: Water hits window pane at 100 km/h

Questions are being investigated experimentally - for example, in a test simulating a wave hitting a window that also was shown on television.

Research engineers wanted to find out whether the window would be destroyed and, in addition, what exactly would happen at the moment of impact. Two drop tests were performed: For the first drop test, the height and amount of water were chosen such that the glass did not suffer damage. The intention of the second drop test during which 1500 liters of water in a balloon were dropped from 38 m height was - in contrast to the television report - to break the window pane with the water balloon at any rate.  Numerical calculations had been made before to meet this requirement.

No conclusive statement can be made about the wave height to which the force of the impact corresponds. However, this test has the advantage that the load is clearly defined and can be simulated using the Finite Element method and correlated with hydro-dynamic calculations.

The aim is to enable sudden loads occurring, for example, in heavy seas and the response of the hull structure to be computed and to identify potential approaches for improving structural design. For this purpose, measured values are compared with calculation results.  Four type PMS40 pressure measurement gauges from HBM were installed on the window. PMS40 pressure measurement gauges are the ideal solution for transient pressure measurements, for example explosions or shock waves - applications where the rise time of the pressure curve is very short and pressure peaks are high.

Genesis HighSpeed measurement data acquisition system

Hamburg-Harburg Technical University opted for HBK's GEN2i mobile data recorder from the "Genesis HighSpeed" series as the data acquisition system to be used. With good reason: The moment the rogue wave hits, a huge amount of measurement data is generated; all of them need to be read out at high resolution to provide detailed insights into the events that took place in these seconds. The GEN2i has been equipped with a bridge amplifier input board offering 1 MegaSample/s sampling rate to enable even the fastest pressure peaks to be detected.

Extreme requirements for the test and measurement equipment - since millions of data per second need to be reliably saved and quickly visualized. These high levels of data processing performance are standard with Genesis HighSpeed:  Perception software enables live data to be visualized on-screen within seconds using patented StatStream technology.  The user has access to raw data instead of modeled information.  Furthermore, data security is top priority - given the fact that it would be difficult or very expensive to repeat tests like this one.

Excellent data security, maximum resolution, fast processing: Reliable test and measurement equipment is a prerequisite for analysis of extreme tests and provides significant results - eventually increasing safety far out at sea.

About TUHH 

The founding principles of the TUHH are unique in Germany: research priority, interdisciplinarity, innovation, regionality as well as internationality are obligatory foundations for our actions. The guiding principle of research, teaching and technology transfer is to develop technology for humanity.

Technology used

Other case studies

Showing 9 of 512 items
No more result to load