arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All Aqira - Test Data Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Structural Qualification of Ariane 5 and 6 Launchers

Spanish National Institute of Aerospace Technology (INTA), Spain

Introduction

HBM helps performing the tests necessary for the structural qualification of the Ariane 5 and 6 launchers.

chevron_left
chevron_right

The Spanish National Institute of Aerospace Technology (INTA), through the Ariane Program Testing Centre (CEPA), is performing the tests necessary for the structural qualification of the Ariane 5 and 6 launchers and as well as for many other elements that will be included in the European Space Agency (ESA) missions.

This requires the most innovative sensor and data acquisition technology to meet the strict requirements in terms of measuring of the dynamic behaviour of the structures, and deadlines.

CEPA uses a combination of HBK strain gauges, the CANHEAD amplifier system, the MGCplus data acquisition system and catman Enterprise DAQ software to acquire information on the structural components of the launchers and to work with up to 7000 simultaneous channels.

The HBK system creates a reliable and versatile measurement chain that provides the maximum precision possible, while reducing cost and test time.

Most importantly ensures the safety of the Ariane launcher and their payloads, thus supporting space projects such as JUICE (Jupiter Icy Moons Explorer).

The Spanish National Institute of Aerospace Technology (INTA) is a public research organization (OPI) under the Ministry of Defence, specializing in technological research and development in the fields of aeronautics, space, hydrodynamics, security and defence.

It has a dual role: to carry out scientific research and system and prototype development activities and provide consultancy services to customers, universities and institutions. Over its more than 75 years of existence, the INTA laboratories and installations have trained many generations of scientists and engineers.

Ricardo Atienza head of CEPA

Further information

chevron_left
chevron_right

Safe Aerospace Missions After the Structural Qualification of the Ariane 5 and 6 Launchers

The Spanish National Institute of Aerospace Technology (INTA), through the Ariane Program Testing Centre (CEPA), carries out the qualification tests on the large structures of the Ariane launchers, specifically those located at the top of the rocket, where the housings are located with the flight control equipment and the interface structure between the first and second launcher stage.

 

CEPA occupies a hangar linked to the airport runway of the Torrejón de Ardoz (Madrid) airbase, and its objective is to ascertain how the launcher and other aircraft structures behave before putting them into operation, and thus help to ensure safety and good performance during flight and operational life.

For this reason, the most innovative technology is required.

 

The testing centre relies on HBK solutions for sensors and data acquisition. In the case of the Ariane 5 and 6 rocket test:

is used to meet the strictest project requirements, regarding both the test quality and deadlines, as there are flight and launch date commitments.

For example, it is envisaged that the space probe for the JUICE (Jupiter Icy Moons Explorer) mission will be launched in 2022 by an Ariane 5 rocket whose structure has already passed the CEPA tests.

The different types of HBK strain gauges and data acquisition systems allow information on the loads to be obtained (by means of hydraulic actuators in order to obtain data for up to 700 tons), working with up to 7000 simultaneous channels.

The strain gauges, present in 80% of the channels, are ideal for measuring the deformation of the structures. The MGCplus and CANHEAD systems, which can be installed near the measuring points, help to reduce the wiring costs and provide an optimal alternative to acquiring and analysing data from a large number of channels.

Furthermore, this HBK solution can be adapted to the needs of each structural qualification testing process, and it meets the requirements of 'large' tests (with between 2000 and 2500 channels, as in the case of the Ariane 6) and 'small' tests (with between 500 and 1000 channels).

Technology used

Other case studies