arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Viking Ship Museum Uses Complete HBK Measurement System

viking ship museum, norway

Introduction

In 2025/2026, a new museum of the Viking Age, which will be an extension of the present Viking Ship Museum, will open on the Bygdøy peninsula in Oslo and, as part of this exciting new project, preparations are already underway to ensure safe handling of the ships and artefacts during the move.

The Viking Ship House within the Museum of Cultural History, which is part of the University of Oslo, houses three Viking era burial ships that were found as part of archaeological finds from Tune, Gokstad (Sandefiord), Oseberg (Tønsberg) and the Borre mound cemetery.

Built as an extension of the present Viking Ship Museum, the new 13,000 m2 building will provide a complete picture of the Viking Age, with the three magnificent ships as the main attraction. Featuring a regulated climate and new support system, the new building will secure the museum’s unique artefacts safely and securely for years to come.

Unique Project by the Viking Ship Museum in Norway Uses Complete Measurement System From HBK

chevron_left
chevron_right

In preparation for the project, the museum’s specialist conservation and collection management staff have been closely collaborating with Statsbygg, the Norwegian Government’s key advisor in construction and property affairs, and external experts to ensure the safe handling of the ships and artefacts, both during the construction process and transition to the new building. However, before this can take place, the ships need to be accurately weighed and this is where HBK was able to step in and help.

Weighing the ships has three main purposes: to determine the total weight; to establish weight distribution; and to monitor changes over time, such as moisture absorption, which can lead to changes in shape. Viewed together with different 3D scanning methods, the ability to monitor the weight distribution will also enable museum staff to understand any potential changes to the ships and effectively remedy them.

Meeting the Need

To move the ships safely and securely, a steel rig will be built around them and a temporary rail system will be laid down. From here, the ships will be lowered down to the new exhibition area. However, before the steel ring can be created, engineers need to collate adequate data. Moving and weighing ships can often be a challenging task as changes in loads or stresses must be minimised or preferably eliminated. To address this, engineers on this project identified many lifting/weighing points and ensured that these points were placed in locations already bearing load. 

In practice, this meant fastening load cells on all vertical supports, and carefully selecting where to place them on the keel support beam, which is the large, shaped beam upon where the ships’ keel rests. Furthermore, to avoid any new stresses, all load cells were placed in pairs.

On the vertical supports, a split bar was clamped to transfer force to the load cells via threaded rods. Angular brackets were also screwed to the side of the keel beam with two 12mm threaded rods connecting the two brackets. Vertical threaded rods again transferred the load to the load cells. When everything was in place, engineers slowly lifted the ship 2.5mm by carefully turning the nuts on these rods in a pre-planned sequence. This was enough to establish weight.

However, when the time came to weigh the bigger Gokstad ship, there were some additional challenges, and this is where HBK was able to help. As weighing points along the keel support beam were being utilised in the moving rig, instead of fastening the brackets that transfer force to the load cells with screws and two approximately placed 12mm rods, engineers needed to use three 24mm hardened steel rods at the lifting point. As these had to be placed with high precision, large holes had to be carefully drilled, whilst causing minimum vibration to the ship.

For this project, Z6 load cells from HBK were installed on various measuring points and connected to a QuantumX MX1615B Strain Gauge Amplifier with catman® AP software.

For such a prestigious project, it was important that we choose the right equipment for the job and that’s why we turned to HBK”,

explains Anders Helseth Nilsson, Department of Collection Management, Museum of Cultural History.

null
null
null

In addition to delivering an exceptional product that met the demands of the task, HBK also delivered the customer service to match, both in terms of the design and quickly solving any issues we had along the way”.

The MX1615B is part of the QuantumX family that offers compact strain gauge amplifiers that deliver accurate results for both dynamic and static measurements. Suitable for precise and safe data acquisition of strain gauges in full-bridge, half-bridge, and quarter-bridge configuration, as well as strain gauge-based transducers, potentiometers, resistance thermometers (PT100) or normalised voltage (+/-10V), the MX1615B is ideal choice whenever strains, forces and displacements are acquired. Equipped with 16 sensor inputs and arranged in compact housing, typical application areas include static stress tests for FEM models, quasi-dynamic fatigue tests for life analysis, monitoring tasks, material investigations, residual stress analysis, maintenance tasks, as well as for general recording of the load data in the field.  Used with catman® AP software, simple data analysis can be achieved.

Following previous experience with another system whereby hardware had performed considerably better than software, the QuantumX with catman® AP software provided the museum with a complete system which is enabling it to continue to achieve accurate and reliable results.

null
null

The Viking Ship Museum is a national symbol, that houses what is probably one of Norway’s most important contributions to world cultural heritage, so concerns surrounding the move have always been of considerable interest. However, thanks to HBK’s extensive experience in weighing technology and demanding fields, it was able to provide a reliable and integrated solution that is enabling the Viking Ship Museum to achieve the results it needs to set sail onto the next stage of this significant project.

Conclusion

To cope with the demand required of this large scale and complex project, the versatility of the QuantumX, combined with the ease of use of the catman® AP software has proved itself to be a valuable resource by enabling the museum to prepare for the next stage of its exciting new journey.

Related Content

No more result to load